2024-02-14 12:51 AM
I haven't seen a 'Mark all as read' option - am I just not looking in the right place?
ie, how to un-bold all of these - without having to open each one individually:
2024-02-14 05:19 AM - edited 2024-02-14 05:21 AM
Hi @Andrew Neil,
The "mark all as read" function is available on board levels.
The screenshot below is taken from the URL:
https://community.st.com/t5/stm32-mcus-products/bd-p/stm32-mcu-products-forum
Is this a functionality you would like to have on the front page as well?
Best regards,
Laurids
2024-02-14 05:23 AM
So I'd have to go down to each board, and click it on each one?
I think there also needs to be a Global one.
2024-02-14 05:26 AM
It says:
So that's a bit misleading - it should really say, "We marked all posts on this board as read."
2024-05-13 06:19 AM - edited 2024-05-13 07:40 AM
@Laurids_PETERSEN wrote:Is this a functionality you would like to have on the front page as well?
Yes, please.
There are so many boards that having to go into each one and do 'Mark all as read' is very tedious.
Example:
So to clear those 4 items requires
2024-06-24 06:24 AM
@Andrew Neil wrote:There are so many boards that having to go into each one and do 'Mark all as read' is very tedious.
Especially when - like today - the forum is running slowly.
☹️
2024-06-24 06:42 AM
Hi @Andrew Neil ,
As @Laurids_PETERSEN mentioned, there is currently no quick fix for this solution, as it is not built in.
I will further check this potential upgrade and let you know once I have more news.
Greetings,
Lina
2024-06-24 06:44 AM
@Andrew Neil , can you please provide .HAR file so we can look into it?
See how to download & PM me afterwards:
ST community site often very slow / unusable - STMicroelectronics Community
2024-06-24 08:24 AM
@Lina DABASINSKAITE wrote:PM me afterwards
The DM composition editor doesn't have a 'Drag and drop here or browse' area to attach files - so how do I do that?
Simply dragging & dropping into the window doesn't work: