cancel
Showing results for 
Search instead for 
Did you mean: 

Is there a 'Mark all as read' ?

Andrew Neil
Super User

I haven't seen a  'Mark all as read' option - am I just not looking in the right place?

ie, how to un-bold all of these - without having to open each one individually:

AndrewNeil_0-1707900612303.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
10 REPLIES 10
Laurids_PETERSEN
Community manager

Hi @Andrew Neil,

The "mark all as read" function is available on board levels.
The screenshot below is taken from the URL: 
https://community.st.com/t5/stm32-mcus-products/bd-p/stm32-mcu-products-forum 

mark all as read.png


Is this a functionality you would like to have on the front page as well?

Best regards,
Laurids

So I'd have to go down to each board, and click it on each one?

I think there also needs to be a Global one.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

It says:

AndrewNeil_0-1707917144029.png

So that's a bit misleading - it should really say, "We marked all posts on this board as read."

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

@Laurids_PETERSEN wrote:

Is this a functionality you would like to have on the front page as well?


Yes, please.

There are so many boards that having to go into each one and do 'Mark all as read' is very tedious.

Example:

AndrewNeil_0-1715610918012.png

So to clear those 4 items requires

  1. Go to the 'Power Management' section
  2. Mark all 
  3. Wait for the confirmation
  4. Return to overview
  5. Go to the 'STM32 MCUs Embedded software' section
  6. Mark all 
  7. Wait for the confirmation
  8. Return to overview
  9. Go to the 'STM32 MCUs Boards and hardware tools' section
  10. Mark all 
  11. Wait for the confirmation
  12. Return to overview
  13. Go to the 'Interface and connectivity ICs' section
  14. Mark all 
  15. Wait for the confirmation
  16. Return to overview

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

@Andrew Neil wrote:

There are so many boards that having to go into each one and do 'Mark all as read' is very tedious.


Especially when - like today - the forum is running slowly.

:frowning_face:

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Hi @Andrew Neil , 

As @Laurids_PETERSEN mentioned, there is currently no quick fix for this solution, as it is not built in. 

I will further check this potential upgrade and let you know once I have more news. 

Greetings,
Lina


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

@Andrew Neil , can you please provide .HAR file so we can look into it? 

See how to download & PM me afterwards:
ST community site often very slow / unusable - STMicroelectronics Community


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

@Lina_DABASINSKAITE wrote:

PM me afterwards


The DM composition editor doesn't have a 'Drag and drop here or browse' area to attach files - so how do I do that?

AndrewNeil_0-1719242620346.png

 

Simply dragging & dropping into the window doesn't work:

AndrewNeil_1-1719242638923.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User

Any update on this?

It remains really tedious to have to go to each board individually, then back to the main listing.

eg, this morning:

AndrewNeil_0-1736503868638.png

So, to clear just 5 posts, I have to:

  1. Go to the 'Others: hardware & software' board
  2. Once there, do 'Mark All as Read'
  3. Wait for that to complete
  4. Go back to the top list
  5. Go to the 'STM8 MCUs' board
  6. Once there, do 'Mark All as Read'
  7. Wait for that to complete
  8. Go back to the top list
  9. Go to the 'STM32CubeIDE (MCUs)' board
  10. Once there, do 'Mark All as Read'
  11. Wait for that to complete
  12. Go back to the top list
  13. Go to the 'STM32 MCUs Motor Control' board
  14. Once there, do 'Mark All as Read'
  15. Wait for that to complete
  16. Go back to the top list
  17. Go to the 'MEMs (sensors)' board
  18. Once there, do 'Mark All as Read'
  19. Wait for that to complete
  20. Go back to the top list

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.