2024-11-06 2:37 AM
Hello. I have made with ST Edge AI Developer Cloud a model and downloaded the whole project for STM32CubeIDE.
When I do Validate on desktop it works fine and I get expected results.
But Validate on target gives me a compilation error.
Building project
Generating project
Temporary project loaded
Temporary AI configuration done
Generating temporary project code
Building project
C:/ST/STM32CubeIDE_1.16.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.200.202406191623/tools/bin/arm-none-eabi-gcc -c -mcpu=cortex-m4 -mfpu=fpv4-sp-d16 -mfloat-abi=hard -DDEBUG -DUSE_HAL_DRIVER -DSTM32G491xx -D -IDrivers/CMSIS/Device/ST/STM32G4xx/Include -IDrivers/CMSIS/Include -IDrivers/STM32G4xx_HAL_Driver/Inc/Legacy -IDrivers/STM32G4xx_HAL_Driver/Inc -IInc -IMiddlewares/ST/AI/Inc -O3 -Wall -fdata-sections -ffunction-sections Drivers/STM32G4xx_HAL_Driver/Src/stm32g4xx_hal.c -o Debug/Drivers/STM32G4xx_HAL_Driver/Src/stm32g4xx_hal.o
<command-line>: error: macro names must be identifiers
In file included from Drivers/STM32G4xx_HAL_Driver/Inc/stm32g4xx_hal_rcc.h:27,
from Inc/stm32g4xx_hal_conf.h:212,
from Drivers/STM32G4xx_HAL_Driver/Inc/stm32g4xx_hal.h:29,
from Drivers/STM32G4xx_HAL_Driver/Src/stm32g4xx_hal.c:35:
Drivers/STM32G4xx_HAL_Driver/Inc/stm32g4xx_hal_def.h:29:10: fatal error: stm32g4xx.h: No such file or directory
29 | #include "stm32g4xx.h"
| ^~~~~~~~~~~~~
compilation terminated.
make: *** [Makefile:75: Debug/Drivers/STM32G4xx_HAL_Driver/Src/stm32g4xx_hal.o] Error 1
Automatic build and run failed
So it does not compile successfully with the no such file or directory for stm32g4xx.h
I have made zero changes to the downloaded project from Developer cloud. And when I try and compile the project myself, it does so successfully.
Solved! Go to Solution.
2024-11-13 1:40 AM - edited 2024-11-13 1:41 AM
Hello,
Validation process expects your board to be in "Waiting (State 1)" state but it seems that it failed to "Error (State 4)" state.
Interestingly, with the .elf file in your project, it hangs on my board (NUCLEO-G474RE). However, while re-generating and compiling your project (with this tweak) on my side, it performs correctly on the target.
Could you please give it a shot by:
- Opening your project in STM32CubeMX
- Go to "X-CUBE-AI"
- select your network ("network" tab)
- Go to Advanced Settings
- Go to "Memory Pools" tab
- Remove "POOL_0_RAM" by clicking "delete" and click on "insert". You should have a new pool named "pool1".
After that, you can either retry a "Validation on target" or generate your project and flash it with STM32CubeProgrammer.
Best regards,
Yanis
2024-11-06 7:17 AM
Hello,
Is it possible to share your version of STM32CubeMX and maybe your project ?
It looks like it does not include automatically the HAL from your target.
Best regards,
Yanis
2024-11-06 7:31 AM
2024-11-06 7:49 AM
>>It looks like it does not include automatically the HAL from your target.
Failure on the Include Paths most likely, double check what's passed in, and the Environment Variables
2024-11-06 11:51 PM
Hi,
Since you answered with STM32CubeIDE version, are you using STM32CubeMX embedded in STM32CubeIDE ? If yes, could you please install STM32CubeMX directly and try the same action with the standalone tool ? You can open the IOC file directly in STM32CubeMX.
STM32CubeMX - STM32Cube initialization code generator - STMicroelectronics
As @Tesla DeLorean said, it might be a include path or missing files. However, since it is from the automatic validation on target action, user does not have any action to do to include these files. We were aware of issues when code generation was performed with STM32CubeMX inside STM32CubeIDE, that's why my proposal is to perform it with the standalone tool.
As a second action, you could switch your application from "SystemPerformance" to "Validation", generate a project, compile/flash and do "Validation on target" without automatic compilation.
Best regards,
Yanis
2024-11-07 2:11 AM
Hi again. Thanks for your input.
I tried it with latest MX version and there it compiles successfully.
Building project
Generating project
Temporary project loaded
Temporary AI configuration done
Generating temporary project code
Building project
Create.
Opening 'mxAI1071861028699'.
10:59:41 **** Build of configuration Debug for project mxAI1071861028699 ****
make -j16 all
arm-none-eabi-gcc -mcpu=cortex-m4 -g3 -DDEBUG -c -x assembler-with-cpp -MMD -MP -MF"Startup/startup_stm32g491retx.d" -MT"Startup/startup_stm32g491retx.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Startup/startup_stm32g491retx.o" "../Startup/startup_stm32g491retx.s"
arm-none-eabi-gcc "../Src/aiPbIO.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DDEBUG -DUSE_HAL_DRIVER -DSTM32G491xx -c -I../Inc -I../Middlewares/ST/AI/Inc -I../Drivers/STM32G4xx_HAL_Driver/Inc -I../Drivers/STM32G4xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32G4xx/Include -I../Drivers/CMSIS/Include -Os -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Src/aiPbIO.d" -MT"Src/aiPbIO.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Src/aiPbIO.o"
arm-none-eabi-gcc "../Src/aiPbMemRWServices.c" -
.
.
continous compilation
.
.
Exec/report summary (validate)
------------------------------------------------------------------------------------------------------------------------
model file : C:\Users\danne\OneDrive\Skrivbord\ai2\NUCLEO-G491RE\sine_model1.tflite
type : tflite
c_name : network
compression : lossless
options : allocate-inputs, allocate-outputs, multi-heaps
optimization : balanced
target/series : stm32g4
memory pool : C:\Users\danne\AppData\Local\Temp\mxAI_workspace11729533689007102031768400636249\mempools.json
workspace dir : C:\Users\danne\AppData\Local\Temp\mxAI_workspace11729533689007102031768400636249
output dir : C:\Users\danne\.stm32cubemx\network_output
vinput files : C:\Users\danne\OneDrive\Dokument\validation_data_no_header.csv
vinput files : C:\Users\danne\OneDrive\Dokument\y_test_output_no_header.csv
voutput files : C:\Users\danne\OneDrive\Dokument\y_test_output_no_header.csv
model_fmt : float
model_name : sine_model1
model_hash : 0xcbda45f1585bf3d837013bae283118d6
params # : 321 items (1.25 KiB)
------------------------------------------------------------------------------------------------------------------------
input 1/1 : 'serving_default_keras_tensor_80', f32(1x1), 4 Bytes, activations
output 1/1 : 'gemm_2', f32(1x1), 4 Bytes, activations
macc : 353
weights (ro) : 1,284 B (1.25 KiB) (1 segment)
activations (rw) : 128 B (128 B) (1 segment) *
ram (total) : 128 B (128 B) = 128 + 0 + 0
------------------------------------------------------------------------------------------------------------------------
(*) 'input'/'output' buffers can be used from the activations buffer
Memory-pools summary (activations/ domain)
--------------- ---- ---------------------- ---------
name id used buffer#
--------------- ---- ---------------------- ---------
POOL_0_RAM 0 128 B (0.1%) 6
weights_array 1 1.25 KiB (128400.0%) 6
--------------- ---- ---------------------- ---------
Running the TFlite model...
INFO: Created TensorFlow Lite XNNPACK delegate for CPU.
Running the STM AI c-model (AI RUNNER)...(name=network, mode=TARGET)
STM Proto-buffer protocol 3.1 (SERIAL:COM3:115200:connected) ['network']
Summary 'network' - ['network']
----------------------------------------------------------------------
inputs/ouputs : 1/1
input_1 : f32[1,1,1,1], 4 Bytes, activations
output_1 : f32[1,1,1,1], 4 Bytes, activations
n_nodes : 5
compile_datetime : Nov 7 2024 10:59:46
activations : 128
weights : 1284
macc : 353
----------------------------------------------------------------------
tools : Legacy ST.AI 1.0.0 - Proto Buffer msg v3.1
runtime lib : 9.1.0 compiled with GCC 11.3.1
capabilities : IO_ONLY, PER_LAYER, PER_LAYER_WITH_DATA
device : stm32 family - 0x479 - STM32G491 @170/170MHz
fpu
----------------------------------------------------------------------
INTERNAL ERROR: E801(HwIOError): Invalid state: 4 instead 1
Validation ended
The warnings are about _close, _fstat, _isatty, _kill aren’t implemented.
I get INTERNAL ERROR which I don't understand, so still, Validate on target has problems.
2024-11-11 3:59 AM
Hello.
No, unfortunately I was not able to solve it.
I am really surprised that there is no simple guide that can show step by step how to deploy a model.
That really is something missing.
2024-11-13 1:40 AM - edited 2024-11-13 1:41 AM
Hello,
Validation process expects your board to be in "Waiting (State 1)" state but it seems that it failed to "Error (State 4)" state.
Interestingly, with the .elf file in your project, it hangs on my board (NUCLEO-G474RE). However, while re-generating and compiling your project (with this tweak) on my side, it performs correctly on the target.
Could you please give it a shot by:
- Opening your project in STM32CubeMX
- Go to "X-CUBE-AI"
- select your network ("network" tab)
- Go to Advanced Settings
- Go to "Memory Pools" tab
- Remove "POOL_0_RAM" by clicking "delete" and click on "insert". You should have a new pool named "pool1".
After that, you can either retry a "Validation on target" or generate your project and flash it with STM32CubeProgrammer.
Best regards,
Yanis
2024-11-13 11:33 PM
Yes thanks it worked here too!
2025-02-20 3:58 AM
Hello... When i opened setting and memory pools, the "POOL_0_RAM" option is not available, instead the memory pools is empty..
After i click on insert and applied it, the same thing happens with the model... What to do???
Please solve my issue....:(