cancel
Showing results for 
Search instead for 
Did you mean: 

Deploying deep learning model on nucleo-H753ZI Validation on target error

Screenshot 2025-02-19 224520.png

 It is fine until validation on desktop... But when it comes to validation on target, the above shown error is displaying...
Can anyone please help me with this error... I am trying this since 3 months...

1 ACCEPTED SOLUTION

Accepted Solutions

Hello @Pinagadi_Meghana ,

 

Indeed, you need to enable to enable the "Automatic compilation and download" to flash the validation firmware in the N6 for the validation on target to work. 

In my case, I am using STM32CubeIDE:

JulianE_0-1740055525507.png

 

Thank you very much @ahsrabrifat for your help!

 

Have a good day,

Juian


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3

Hello @Pinagadi_Meghana ,

 

Indeed, you need to enable to enable the "Automatic compilation and download" to flash the validation firmware in the N6 for the validation on target to work. 

In my case, I am using STM32CubeIDE:

JulianE_0-1740055525507.png

 

Thank you very much @ahsrabrifat for your help!

 

Have a good day,

Juian


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

What are the options that i need to give at communication port, TX pin and RX pin...
when i selected them  by looking at the pinout configuration, it is saying that no board is connected...???
i will share the screenshot of it please have a look