Hello,Indeed, templates from ST Edge AI Developer Cloud do not contain any code related to camera interface. It provides ready-to-try templates to run inference on the target based on model, parameters, and memory configuration of a given target. Bas...
Hello,It probably means X-CUBE-AI plugin was not able to contact distant server in order to download it.Based on your screenshot, you can install it manually from the zip. Here are the steps:- Go to https://www.st.com/en/embedded-software/x-cube-ai.h...
Hello,The tool shows accuracy (acc column) means "Classification accuracy". If it is not displayed, it means we were not able to detect your model as a classifier. You can still force this flag with '--classifier' or through the "Advanced Settings" i...
Hello,You have the ability to plug a camera in STM32H7S78-DK so you should be able to make applications like Face Recognition.You could go with your own application code on STM32H7S78-DK and get inspiration of the function pack (it is not officially...
Hello,Actually FP-AI-VISION function pack implementation only supports STM32H747I-DISCO. I would recommend to stay with STM32H747I-DISCO if your goal is to run FP-AI-VISION. Best regards