When I configure ADC1 to read voltage input from PA0 and PA1 using DMA, then the behavior is as below in each condition1) PA0 = 0 (GND) ; PA1 = variable pot (0-5V)then PA1 provides values as per input from pot but max value displayed in 3022 instead ...