Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

udestk CMD -Solve the cause of unstable automatic burning

1.Introduction to automated programming: IC:SPC58NN Cmd:C:\Program Files (x86)\pls\UDE 5.2\MemtoolCli.exe PROGRAM "D:\EOL_SAIC_PICU_PI11_7E07E8_20231019_CRC_Sim_HSM.hex" Error:Please refer to the attachment. e-mail:medinalv@sinbon.com

5df75fcb06bb0a21ae903bf3fceaf56.jpg
medinaLv by Associate
  • 1571 Views
  • 0 replies
  • 0 kudos

Resolved! SPC570S CAN Message Filter

Hello,I am struggling with the individual RX CAN Message Filter RXIMRx on SPC570S.First Question:Is there an Application Note available for the SPC57x Note like it is for the for SPC58x (TN1348).Second Question:I want to use the RX CAN Message Filter...

MFisc.3 by Associate
  • 2370 Views
  • 2 replies
  • 1 kudos

EVAL-L9788 with SPC57K-Line MCU

Hello,I am working on SPC57K-Line MCU with IC L9788. I want to use also GUI to configure and control L9788 through the MSC bus. But I always see this error "Failed to reset MONACO". I tested COM port and UART connection and all connections are correc...

angela__0-1710943379950.png
angela_ by Associate
  • 1216 Views
  • 0 replies
  • 0 kudos

Need to Flash the program every time i power up my board

Hi, I've made a custom board using an SPC5 microcontroller for my automotive-based application, but I've been facing the issue that I need to flash my code with my external SPC5 debugger every time I power up my board, and then only it starts working...

SV.9 by Associate II
  • 1932 Views
  • 1 replies
  • 1 kudos