Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SPC5Studio IVOR2/3 Handler

Posted on November 07, 2016 at 06:10Hi,Has anyone used IVOR2/3 Handler using SPC5Studio? I would like to how to write IVOR2/3 Handler routine using SPC5Studio.Thanks and Regards,Dinesh Rode

dinesh by Associate
  • 1116 Views
  • 1 replies
  • 0 kudos

SPC5Studio Build and Debug Problems

Posted on October 31, 2016 at 12:57Hello,I'm new to SPC5Studio environment and experiencing some problems using it. I'll be glad if you can help about the following issues:1) When I try to create a project using steps ''File->New->C Project->Makefil...

evren by Associate
  • 1108 Views
  • 1 replies
  • 0 kudos

Importing SPC5Studio V3.5 project using V5.0

Posted on October 27, 2016 at 14:46Hi,I need to work on old project created using SPC5Studio V3.5. Project is created using Wizards. When I open same project using V5.0, the 'Configuration.xml' is showing some error (red cross against file name). If...

dinesh by Associate
  • 948 Views
  • 1 replies
  • 0 kudos

Running code from SRAM through BAM loader

Posted on October 17, 2016 at 21:10Hello, Does SPC5Studio provide a way to configure the toolchain to link code to the appropriate address to run from the BAM bootloader, or should I just modify the generated application.ld as I see fit? My goal is ...

SPC5 studio - placing variables at fixed RAM addresses

Posted on September 27, 2016 at 10:54Hello everyone.I�m working on a Bolero microcontroller (SPC560D40L3) using SPC5Studio and Hightec Compiler.I have a question related to variables to be located in RAM.I have a set of global variables, which I nee...

SPC563M64 JATG uncensoring through USB Multilink

Posted on October 13, 2016 at 23:50Hi all. I have some trouble to connect SPC563M64 through USB Multilink. My device is in censored mode with configuration 0xAAAA_AAAA and serial password 0x1122334455667788. I try to uncensor device with this passwo...

cbnsspb by Associate
  • 1233 Views
  • 1 replies
  • 0 kudos

PLS UDE and Windows 10

Posted on September 21, 2016 at 11:28Dear All ,in case of Connexion issues with PLS (FTDI Issues) and Discovery Board.Please , install the the last software (4.07.04) coming from PLS websitehttp://www.pls-mc.com/download-spc5-udestk/downloads-a-1626...

Use of timers with large software

Posted on September 13, 2016 at 15:16Good day to everyone,I am writing here in order to have some suggestions on the use of timers. I am writing a spc5 application whee I have a lot of operations and I must do various things at specific moments. For...

Help For using Os in SpcStudio

Posted on August 28, 2016 at 10:16Hi I have new Project , for this project i want to use an OS for my core I don't know how can i use this oses and are they have any license for using in spcstudio ? Thanks For Help With Best Regards Nazerian Vani...

Write An assembly code in spcstudio

Posted on August 28, 2016 at 10:08Hi I want to write some asm instruction in Spc studio but i don't know how can i write these instructions. if there is exist any sample please let me know about this sample. Thanks With Best Regards Nazerian Vanim...