2024-11-28 05:39 AM - last edited on 2024-11-28 05:43 AM by Andrew Neil
Dear community,
I am exploring the use of AutoDevKit for the battery management of my battery in my project. I watched all videos and read through the manual for the AEK-POW-BMS63EN. However, I am new to this environment and need some help with the following procedure.
Thank you very much for your help.
Camillo
2024-11-28 05:43 AM
Hi,
Yes, the best is to start using our HW and SW and import an existing project(s) from AutoDevKit.
Because the source code is all visible, you can first run it and then put it in debug mode by setting breakpoints to understand the internal logic.
Only after these steps are completed, you can start defining a new BMS application by creating a new AutoDevKit project and adding the BMS Chain components.
Best Regards,
AutoDevKit Team
2024-11-28 05:55 AM
Hello Mr. Vizzini,
thank you very much for your help. Is the SPC58EC – AEK_POW_BMS63EN_SOC_Estimation_Single application for discovery demo a good starting point? Or do you suggest another demo?
Best regards,
Camillo
2024-11-28 05:59 AM
Hi,
Please use the new driver version 'CHAIN'
Best Regards,
AutoDevKit Team
2024-11-28 06:03 AM
Hello Mr. Vizzini,
my board is the BMS63EN and not the BMSWTX. Is there a different procedure or does it work the same?
Kind regards,
Camillo
2024-11-28 07:53 AM
Hi,
AEK-POW-BMS63EN + AEK-COM-ISOSPI1 is equivalent to AEK-POW-BMSWTX.
From HW point of view, either you use the 2 boards, or you use a single board.
Both configurations need to be connected with MCU (AEK-MCU-C4MLIT1).
If you need a battery holder, you can use AEK-POW-BMSHOLD (14 cells in series, one full BMS node).
Best Regards,
AutoDevKit Team