2023-12-13 10:06 AM
I had a fine working setup with BMS63 for some hours.
Than cell 12 showed 0V and the fault light in the ISO SPI came up.
A short measurement showed, the cell was indeed empty (I am testing with very old cells).
After replacing the cell cell 12 still shows 0V, and the fault light is still on.
If I measure with the testpins on the BMS63EN itself, I can see that there is a cell voltage. So something went wrong with the BMS63EN I think.
Do I need to reset the error/fault? In the manual its stated that software diagnostics need to be run in such case. But..how?
And shouldn´t that be all reset after a complete disconnect and new init?
Solved! Go to Solution.
2023-12-15 07:37 AM
Hi Orbiter,
In order to print on Serial terminal diagnostic info please replace main_core0 function with:
void main_core0(void) {
char message[15];
AEK_POW_BMS63EN_module_t AEK_POW_BMS63EN_BatteryModule;
uint8_t cell_idx = 0;
/* Enable Interrupts */
irqIsrEnable();
sd_lld_start(&SD5,&serial_config_BMS_serial);
/* Application main loop.*/
for ( ; ; ) {
if((osalThreadGetMilliseconds()%100)==0){
AEK_POW_BMS63EN_BatteryModule = AEK_POW_BMS63EN_GetModule(i_device_disp);
//SOC Elaboration Done
sprintf(message, "DEV:%d \n", (int)(i_device_disp+1));
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
//Printing SOC
for(cell_idx = AEK_POW_BMS63EN_CELL1; cell_idx <= AEK_POW_BMS63EN_CELL14; cell_idx ++){
sprintf(message, "T%.2d:%.3f ", cell_idx+1, AEK_POW_BMS63EN_BatteryModule.AEK_POW_BMS63EN_Pack_CellTemperatureNTC[cell_idx]);
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
}
sprintf(message," \n");
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
//Printing Bal
for(cell_idx = AEK_POW_BMS63EN_CELL1; cell_idx <= AEK_POW_BMS63EN_CELL14; cell_idx ++){
sprintf(message, "B%.2d:%.3d ", cell_idx+1, AEK_POW_BMS63EN_BatteryModule.AEK_POW_BMS63EN_Pack_Bal_cmd[cell_idx]);
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
}
sprintf(message," \n");
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
//Printing Voltage
for(cell_idx = AEK_POW_BMS63EN_CELL1; cell_idx <= AEK_POW_BMS63EN_CELL14; cell_idx ++){
sprintf(message, "V%.2d:%.3f ", cell_idx+1, AEK_POW_BMS63EN_BatteryModule.AEK_POW_BMS63EN_Pack_CellVoltage[cell_idx]);
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
}
sprintf(message," \n");
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
//Printing Current
sprintf(message, "C:%.4f \n", AEK_POW_BMS63EN_BatteryModule.AEK_POW_BMS63EN_Pack_Current);
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
//Printing Current
sprintf(message, "F1:%d \n", AEK_POW_BMS63EN_BatteryModule.AEK_POW_BMS63EN_Fault1_data);
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
sprintf(message, "F2:%d \n", AEK_POW_BMS63EN_BatteryModule.AEK_POW_BMS63EN_Fault2_data);
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
sprintf(message, "VOV:%d \n", AEK_POW_BMS63EN_BatteryModule.AEK_POW_BMS63EN_VcellOV_Fault_data);
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
sprintf(message, "VIUV:%d \n", AEK_POW_BMS63EN_BatteryModule.AEK_POW_BMS63EN_VcellUV_Fault_data);
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
sprintf(message, "OVL:%d \n", AEK_POW_BMS63EN_BatteryModule.AEK_POW_BMS63EN_OverLatch);
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
sprintf(message, "GPIOF:%d \n", AEK_POW_BMS63EN_BatteryModule.AEK_POW_BMS63EN_GPIOOTUT_Fault_data);
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
}
}
}
Moreover, please, make sure that cell 9 is connected to cell 12.
Best Regards,
AutoDevKit Team.
2023-12-13 10:57 AM - edited 2023-12-13 11:02 AM
Follow up... how would one output any diagnostic error?
I can´t get the RLA Serial example to output any meaningful text- so I am a bit puzzled on how to easily use the console as well.
Is there a part II of the UM "getting started with BMS63EN"? There are so many things going on in the basic example.. The doxygen documents are not explaining, aren´t they? And the L9963E datasheet is on bit level. Maybe I look in the wrong places?
2023-12-14 06:30 AM
Hi Michael,
The debug is done with a console terminal (e.g. teraterm) on a PC connected via USB to the AEK-MCU-C4MLIT1.
After plugging the USB cable, you should see a COM port enabled in your PC drivers. If not, there could be some issues with your FTDI drivers in your PC.
In the BMS example, the second core is devoted to send the signal to the terminal via the serial COM port. If you look at the code, there is the reading of the data and diagnostic errors (faults 1, faults 2, etc.) and "printing" on the serial port.
This will work only if the battery are properly connected otherwise the second core will see only empty values.
Therefore, the question becomes how did you connect the battery cells? Did you make sure that the first two and the last two are connected as indicated in the user manual?
Please be reminded that L9963E is supplied from the same batteries, therefore if the connection is not correct the ISOSPI communication will not work.
I am not sure what you mean with "old cells"... I hope they are not out from the accepted values.
Best Regards,
AutoDevKit Team
2023-12-14 08:12 AM
Hi Max!
Terminal? Is this the same as the use of the serial terminal in Autodevkit? COM Port and 115200? That is what I used so far. I just checked with Putty, I get the same output there. Picture attached.
I looked for the diagnostic reading in the code, but I could not find it... I just found that the main() calls AEK_POW_BMS63EN_Start_Mgn_exec(); which also runs if(AEK_COM_ISOSPI_GetFault(ISOSPI_DEV0)){
AEK_POW_BMS63EN_DIAG_Measurement();.
But that function just writes the fault data into AEK_POW_BMS63EN_BatteryModules[AEK_POW_BMS63EN_DEVICE(dev)].AEK_POW_BMS63EN_Fault1_data
}
But in the main on core 0 this data is never outputed:
Or- did I miss something? (probably)
Cell connection:
I have 12 LiFePo4 Cells, series connected.
I left Cell 10 and Cell11 out on the BMS63EN, so 1-9 and 12-14 are connected to the 12 cells on my test system.
Old cells...means old cells, they are all charged up but quite used and some have quite a low capacity left - which is what makes charging and draining a bit faster. But yes-they all are between 2.9 and 3.1V charged right now
LED:
I have the green LED on the BMS on
Green, Blue, Yellow and Red on ISO SPI
Green blinking on the outmost right LED (LED2) on MCLIT4
2023-12-15 07:37 AM
Hi Orbiter,
In order to print on Serial terminal diagnostic info please replace main_core0 function with:
void main_core0(void) {
char message[15];
AEK_POW_BMS63EN_module_t AEK_POW_BMS63EN_BatteryModule;
uint8_t cell_idx = 0;
/* Enable Interrupts */
irqIsrEnable();
sd_lld_start(&SD5,&serial_config_BMS_serial);
/* Application main loop.*/
for ( ; ; ) {
if((osalThreadGetMilliseconds()%100)==0){
AEK_POW_BMS63EN_BatteryModule = AEK_POW_BMS63EN_GetModule(i_device_disp);
//SOC Elaboration Done
sprintf(message, "DEV:%d \n", (int)(i_device_disp+1));
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
//Printing SOC
for(cell_idx = AEK_POW_BMS63EN_CELL1; cell_idx <= AEK_POW_BMS63EN_CELL14; cell_idx ++){
sprintf(message, "T%.2d:%.3f ", cell_idx+1, AEK_POW_BMS63EN_BatteryModule.AEK_POW_BMS63EN_Pack_CellTemperatureNTC[cell_idx]);
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
}
sprintf(message," \n");
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
//Printing Bal
for(cell_idx = AEK_POW_BMS63EN_CELL1; cell_idx <= AEK_POW_BMS63EN_CELL14; cell_idx ++){
sprintf(message, "B%.2d:%.3d ", cell_idx+1, AEK_POW_BMS63EN_BatteryModule.AEK_POW_BMS63EN_Pack_Bal_cmd[cell_idx]);
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
}
sprintf(message," \n");
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
//Printing Voltage
for(cell_idx = AEK_POW_BMS63EN_CELL1; cell_idx <= AEK_POW_BMS63EN_CELL14; cell_idx ++){
sprintf(message, "V%.2d:%.3f ", cell_idx+1, AEK_POW_BMS63EN_BatteryModule.AEK_POW_BMS63EN_Pack_CellVoltage[cell_idx]);
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
}
sprintf(message," \n");
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
//Printing Current
sprintf(message, "C:%.4f \n", AEK_POW_BMS63EN_BatteryModule.AEK_POW_BMS63EN_Pack_Current);
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
//Printing Current
sprintf(message, "F1:%d \n", AEK_POW_BMS63EN_BatteryModule.AEK_POW_BMS63EN_Fault1_data);
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
sprintf(message, "F2:%d \n", AEK_POW_BMS63EN_BatteryModule.AEK_POW_BMS63EN_Fault2_data);
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
sprintf(message, "VOV:%d \n", AEK_POW_BMS63EN_BatteryModule.AEK_POW_BMS63EN_VcellOV_Fault_data);
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
sprintf(message, "VIUV:%d \n", AEK_POW_BMS63EN_BatteryModule.AEK_POW_BMS63EN_VcellUV_Fault_data);
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
sprintf(message, "OVL:%d \n", AEK_POW_BMS63EN_BatteryModule.AEK_POW_BMS63EN_OverLatch);
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
sprintf(message, "GPIOF:%d \n", AEK_POW_BMS63EN_BatteryModule.AEK_POW_BMS63EN_GPIOOTUT_Fault_data);
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
}
}
}
Moreover, please, make sure that cell 9 is connected to cell 12.
Best Regards,
AutoDevKit Team.
2023-12-15 12:26 PM
Ahhhhhh nice, that works, thanks!
The compiler complains a bit:
main.c:114:7: warning: format '%d' expects argument of type 'int', but argument 3 has type 'uint32_t' [-Wformat=]
But I can ignore that and it works.
Can I ask for some help with the debug? This is what I got out of the system:
DEV:1
T01:0.000 T02:0.000 T03:0.000 T04:0.000 T05:0.000 T06:0.000 T07:0.000 T08:0.000 T09:0.000 T10:0.000 T11:0.000 T12:0.000 T13:0.000 T14:0.000
B01:000 B02:000 B03:000 B04:000 B05:000 B06:001 B07:000 B08:000 B09:000 B10:000 B11:000 B12:000 B13:000 B14:000
V01:3.083 V02:3.143 V03:3.110 V04:3.110 V05:3.112 V06:3.151 V07:3.106 V08:3.133 V09:2.858 V10:0.000 V11:0.000 V12:0.000 V13:3.109 V14:3.034
C:0.0003
Fault 1:8
Fault 2:0
VCell 0V:0
VCell UV:2048
Overlatch:1
GPIO Faults:0
So if I understand the datasheet correct this would mean:
- Fault 1:8 -> 1000 -> Bit offset = 3 -> Reads FaultL pin value = Dev1 has detected a fault
- VCell UV:2048 ->offset 11 -> Cell undervoltage detected = a cell triggered undervoltage
- Overlatch active - > What is that? If I run search through the datasheet I can´t find any information for "overlatch" "over latch" "OVL" - so I wonder what that means and how to deal with it.
So, cell 12 does not read any voltage, but I can measure the voltage on the BMS63EN board via testpins.
Cell 9 is connected to cell 12, I get current out of the batterypack and I can measure pack voltage with an external multimeter, so - I am quite sure its connected.
What am I missing?
2023-12-15 01:09 PM
Ahhh Page 91 of the datasheet: ADCV register..
The following fault handling procedure must be executed once configuration override is over:
1. MCU must access diagnostic latches and perform correct failure validation as recommended in
Table 60.
2. MCU must launch On-Demand Conversions (SOC = 1) in order to update measurement registers,
while also disabling any cyclic execution by setting CONF_CYCLIC_EN = 0 in the same SPI frame.
3. MCU must wait for On-Demand Conversions to be over and evaluate routine result by reading the
ADCV_CONV register. A read operation on such a register would reset the OVR_LATCH in case the
execution launched at step 2 ended with no failure:
◦ In case failure persists, the read operation will not reset the OVR_LATCH. Return to step 1.
◦ In case failure disappeared, reading the ADCV_CONV register will also reset the OVR_LATCH.
Proceed to step 4.
4. Read all diagnostic latches in order to clear them.
5. (Optional) Restart any cyclic execution by setting CONF_CYCLIC_EN = 1
But..am I supposed to change registers at this point or is there already a function somewhere?
And to avoid all these questions, how is it intended to find those and other functions?
2023-12-16 01:25 AM
Hi Michael,
There is a full help file for each component with all available functions.
It would make no sense to build a driver and to force the driver user to go change single registers.
right-click on the component, AEK-POW-BMS63EN --> documents --> .chm file (see attached pictures).
In addition, there is UM3185
At page 40 / paragraph 10 you also have the list of main APIs.
I understand that it is easier to ask than read a manual but it in this way it becomes more a co-development than a support...
Thanks.
AutoDevKit Teams
2023-12-17 08:06 AM
Hi Max,
it´s not that I am not trying, I really don´t get behind it.
My BMS is in latched state and has a lit up fault LED and can´t read voltages from cell 12. At least it reads 0V where it should read a voltage inside the defined range.
So I hope thats because its latched.
No matter how often I read, I can´t find the API to reset the latch.
Or does your bms example do all of this by default and the error persist and I need to look somewhere else?
2023-12-17 10:47 AM
I just rebuild the hardware of my test-BMS to narrow it down.
I removed another two cells and connected the remaining cells sense wires together as described in the Datasheet.
According to the cfg.c the changes are correct: