Hi Aishwarya UMThe FDA903D audio amplifier provides the ability to detect the open load even in play.If the audio signal is judged to be good enough to provide a reliable result, the test result is valid. Otherwise, if the audio signal doesn't allow ...
Hi Shiva_ShankarThe FDA903D audio amplifier provides the ability to detect the open load even in play.If the audio signal is judged to be good enough to provide a reliable result, the test result is valid. Otherwise, if the audio signal doesn't allow...
Hello Decemberdream,the pin modes indicate the direction of the signal depending on the micro, i.e. mode_input means that this pin is set as the input pin of the micro, pin_output means that this is a pin from which the signal goes out of the micro. ...
Hi Bwang,In AutoDevKit Studio the pins are set to latched state Low by default, because a low signal can be used to save energy.Of course, the pin configuration can be changed according to the needs of your application.Thanks,AutoDevKit Team