AutoDevKit Ecosystem

Ask questions and find answers on the AutoDevKit solution. Discuss voltage configurations, motor control, and AutoDevKitStudio programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Issue rised during flasing and debugging

Hello Team,I hope this message finds you well.I am reaching out to seek your guidance regarding an issue I am encountering while flashing software. Despite following the standard procedures, I am facing the following errors (as shown in the attached ...

Aishwaryaum_1-1736424682036.jpeg Aishwaryaum_2-1736424690531.jpeg

Resolved! AEK-POW_BMS63EN cell balancing manually adjust

Dear community members, There are multiple functions related to cell balancing in AEK-POW_BMS63EN_id. However, when I tested, none of them work. Here is my main code based on the "SPC58EC - AEK_POW_BMS63EN_SOC_Estimation_14Cells_GUI application for d...

trishuynh_0-1730455880757.png trishuynh_1-1730455908832.png
trishuynh by Associate III
  • 16145 Views
  • 12 replies
  • 0 kudos

Resolved! L9963E Burst frame response error

Dear Community member,In L9963E burst response for 0x78, we are getting only 17 response frames out of 18 after feedback response.Last frame 18 is missing. Also the cell 7,8,9,10 is disable, while it is showing no data(for disable cell) for cell 6,7,...

bitBuddy by Associate II
  • 2406 Views
  • 2 replies
  • 0 kudos

Resolved! AEK_POW_BMS63EN Fault_L_line_status is always 1

Dear Community members,I have connected 2 node in ring configuration, and working on an custom pcb for BMS.In registers Faults1, Fault_L_line_status is always 1, while all other fields of Faults1 and Faults2 registers are 0. Also the OVRLATCH is not ...

bitBuddy by Associate II
  • 4812 Views
  • 6 replies
  • 1 kudos

Resolved! AEK-POW_BMS63EN : Fault pin is not being high

Dear Community members,In an SPC582b-discovery example code, i modified configuration to set over voltage threshold 3.4 v. While all the cells in stack is over than 3.4 but the Fault pin in board is not being high.  Regards,bitBuddy

bitBuddy by Associate II
  • 2223 Views
  • 1 replies
  • 0 kudos