AutoDevKit Ecosystem

Ask questions and find answers on the AutoDevKit solution. Discuss voltage configurations, motor control, and AutoDevKitStudio programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

i want to add delay into my code

hi community,i my project. i am using PIT and it is working fine. before initialization of the drivers osalThreadDelayMilliseconds() is working fine. but after initialization of the low level drivers, osalThreadDelayMilliseconds() is blocked even tho...

Resolved! Regarding OSAL Delay functions

Dear all,Good morning, I am facing issues with some functions in autodevkit.The functions osalThreadDelayMilliseconds() and osalThreadDelayMilliseconds() are blocking the entire execution.As the Autodevkit driver doesn't support the CANTP(response ta...

Resolved! AEK-POW_BMS63EN Current, NTC measurement and fault LED

Dear community members,I have three questions about the AEK-POW_BMS63EN require answers and input from experts:1. After running the example of AEK-POW_BMS63EN, everything is ok; however, the fault LED on  is always high in AEK-COM-ISOSPI1 even though...

trishuynh by Associate III
  • 2849 Views
  • 4 replies
  • 2 kudos

Resolved! Need Help with SPC5 Studio for Basic LED Blinking Program

Hello all,I'm Ali, new to ST Microcontrollers, and I'm seeking some guidance to get started with SPC5 Studio. Previously, I developed custom SDKs where I had control over registers, their addresses, and more. However, transitioning to SPC5 Studio has...

Ali5 by Associate III
  • 4927 Views
  • 6 replies
  • 1 kudos

Resolved! SPC5 Studio

I recently installed SPC5 studio and I'm referring to example codes. The example code is building without errors but there are problems indicating, Description Resource Path Location TypeSymbol 'NULL' could not be resolved main.c /SPC582Bxx_RLA FreeR...

jsw2000 by Associate II
  • 4499 Views
  • 3 replies
  • 1 kudos

Resolved! AutoDevKit does not appears in zip folder.

Hi, I'm an SPC5 beginner. I followed the YouTube tutorial and correctly installed AutoDevKit zip file. When i go SPC5Studio>Help>Install New Software>Add>Local, AutoDevKit does not appears in my unziped folder. I see there are some files in the video...

Nurlan13 by Associate
  • 1698 Views
  • 1 replies
  • 1 kudos