AutoDevKit Ecosystem

Ask questions and find answers on the AutoDevKit solution. Discuss voltage configurations, motor control, and AutoDevKitStudio programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! L9963E meaning of VTREF_BIST_FAIL flag

Hi,The screenshot below is from the L9963E datasheet DS13636, page 125. Is the description for VTREF_BIST_FAIL here a typo?It matches exactly the description of a the VCOM_COMP_BIST_FAIL bit in the BIST_COMP register, which makes more sense. I note t...

abtjmehmet_0-1726654040604.png

Resolved! Regarding sound optimization in AVAS

Hello all,A very good morning, I hope you all have the good day.I am developing the AVAS project taking the base code(shown in the snippet) from the AutoDevKit.Here my requirement is I need to increase the sound from speed 0 to 20kmph and sound shoul...

Aishwaryaum_0-1727416129427.png

Resolved! Issue downloading free license for Hightech Compiler

Hi everyone,I’m trying to download a free license for the Hightech compiler from the following link:https://register.hightec-rt.com/st/spc5x/Unfortunately, the page returns the following error:This page isn’t workingThe site register.hightec-rt.com i...

Mjuchelka by Associate II
  • 2543 Views
  • 2 replies
  • 0 kudos

Resolved! AutoDevKitStudio Pin Map generation

Hi,I have recently started working with AutoDevKitStudio and tried some of the example codes. When I wanted to modify example code and add more pins in Pin Map editor, after saving my changes and generating them I couldn't see newly defined ports in ...

MaraLo by Associate II
  • 2369 Views
  • 3 replies
  • 0 kudos

AVAS - how to load an audio file with OpenOCD

#autodevkit hashtag#avas hashtag#openocd hashtag#mcu hashtag#spc5 hashtag#embedded hashtag#automotiveHere you are a quick guide to help you load the audio file in AEK-AUD-C1D9031 Avas board using the AEK-MCU-SPC5LNK programmer.AEK-AUD-C1D9031 - https...

Resolved! symbol could not be resolved

good morning. i just finished my code that makes a led blink. i pinned it on the GUI and wrote the code on the main. before flashing it i want to know what is the problem of my pin: it is written that the symbol can not be resolved even thougt there ...

Jad_0-1725698648759.png Jad_1-1725698655587.png
Jad by Senior
  • 1361 Views
  • 1 replies
  • 0 kudos

Resolved! led blinking

good morningi want to create a simple led blinking code. for that, i got the path of the led 8 of my aek-mcu-c4mlit1. it is pk1gpio1 and is connected to the branch 25. i connected it on the gui and wanted to code in my main. unfortunately, C recogniz...

Jad_0-1725628089535.png Jad_1-1725628126891.png
Jad by Senior
  • 6252 Views
  • 10 replies
  • 1 kudos

Resolved! SPC582B flashing error

hello team,I'm using AutodevKit studio for testing AEK_AUD_C1D9031 board. I imported example code from sample : SPC582Bxx_RLA_AEK_AUD_C1D9031 - Avas Compact - Test Application.   but upon flashing board I'm getting this error. kindly provide feedbac...

MohitManvar_0-1725527788326.png