Analog and audio

Find useful information on analog and audio applications: TDA7294-based designs, PDM to PCM noise, and SPICE models.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Forum board changes

Dear community member, The “Analog and audio” topic is no longer supported on the ST community. The legacy content is available only by the read-only basis. If you have any requests regarding "Analog and audio”  topics, check the alternative support ...

Resolved! Tsv6395

Hi, Im working on a project which need using a op-amp and a comparator. In that matter I’ve looked at the tsv6395 which have great spec as an op-amp, but i wonder if it is acceptable to use one channel as comparator? the signal is about 100hzThanks f...

Bratland by Associate
  • 2353 Views
  • 2 replies
  • 0 kudos

Resolved! Data sheet for chip marked EZFT V6294AI MRC021?

Hello, and thanks in advance for your help.  I'm trying to debug (repair) an old circuit board on which we have a 14 pin surface mount chip with the labeling, ST EZFT V6294AI MRC021.    Is this one of your chips? If so, is it possible to get a datash...

adc120 channel selection and data issues

hello.I'm currently testing a 2-axis joystick connected to an ADC120.I want the X and Y axis values ​​to go into IN0 and IN1, but only the X axis values ​​go into all channels. The channel changes normally, but is it possible to separately input 2-ax...

WOO by Associate
  • 2535 Views
  • 2 replies
  • 1 kudos

Resolved! Power On Reset of TS334

HelloI would like to confirm with you the power on reset behavior of TS334.When I power up the comparator, I see a high level impulse during power on.I guess there is a power on reset behavior of TS334. In the following figure, the blue curve is the ...

Capture1.PNG TS334_01.png
YFANG.2 by Associate III
  • 2610 Views
  • 2 replies
  • 2 kudos

ATIC224-CC and ATIC224-CA

Dear Support,Please advise what are the differences between part numbersATIC224-CC and ATIC224-CA?KIndly confirm if they can be used interchangeably. Thanks

igamoso by Associate III
  • 2610 Views
  • 2 replies
  • 0 kudos

ADC120 channel selection problem

 Hi,  I use ADC120 my new project, but device get only convert first channel. I change channel but its gives only first ch.There is a ST demo bord at web site but there is a no example code. How can i solve this problem.I read same topic in this web ...