Analog and audio

Find useful information on analog and audio applications: TDA7294-based designs, PDM to PCM noise, and SPICE models.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Forum board changes

Dear community member, The “Analog and audio” topic is no longer supported on the ST community. The legacy content is available only by the read-only basis. If you have any requests regarding "Analog and audio”  topics, check the alternative support ...

Spice Model for TSV6 Op Amps

Posted on May 29, 2012 at 15:24Do you have SPICE models for TSV6390AIDT and/or TSV6290AIDT? Thanks, Luli #op-amps-spice-macromodel

luli755 by Associate
  • 1736 Views
  • 2 replies
  • 0 kudos

Op amp voltage range

Posted on June 06, 2012 at 17:17I am adopting the TS922 family and I have a 16Volt rail on my PCB board. I am thinking to use a rail splitter (+/- 8Volts) or I can always step down the supply voltage if needed. The supply voltage of TS922 listed in ...

z58 by Associate
  • 1300 Views
  • 1 replies
  • 0 kudos

Maximum output current of an OpAmp

Posted on May 04, 2012 at 17:05Hello,In datasheet, sometimes maximum output current is indicated (IsourceMin, Typ, Max), sometimes it is missing.What is the best method to determine if an OpAmp can supply enough current to our load?Thanks for the su...

Op-amps with single supply or dual supply ?

Posted on April 06, 2012 at 10:05Dear forum members,Perhaps, you wonder what is the difference between single and dual supplies ?Or maybe if the op-amp will have the same behavior with Vcc= 0 -> 5V or Vcc= +/- 2.5V.It is important to keep in mind th...

0690X00000604xLQAQ.png 0690X00000604xMQAQ.png 0690X00000604wnQAA.png 0690X00000604xVQAQ.png

Crossref to ST Op Amps

Posted on February 15, 2012 at 12:04Dear forum-users,If you like using ST Op-Amps, here is a simple table that will direct you quickly to the most appropriate ST Op-Amps, based on popular standard devices.  ST Op Amps  Standard devices  Descriptio...

Macromodel location

Posted on December 05, 2011 at 11:19Hello,I would like to use macromodels to simulate my schematics but I am not able to find them.I think that they are available because in the TSV6239 datasheet it is mentioned  :Two accurate macromodels (with or w...

allan by Associate
  • 1887 Views
  • 1 replies
  • 0 kudos

How to select an Operational Amplifier?

Posted on November 18, 2011 at 15:17Dear Forum Members,I�d like to share a few tips on the usual process I use to select an Op Amp based on pre-defined technical requirement.The tool I use more often is the product selector, which can be accessed by...

0690X00000602OiQAI.bmp 0690X00000602fAQAQ.jpg 0690X00000602O5QAI.bmp 0690X00000602PWQAY.bmp