cancel
Showing results for 
Search instead for 
Did you mean: 

Tsv6395

Bratland
Associate

Hi, 

Im working on a project which need using a op-amp and a comparator. In that matter I’ve looked at the tsv6395 which have great spec as an op-amp, but i wonder if it is acceptable to use one channel as comparator? 

the signal is about 100hz

Thanks for any advice,

Mg

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
AScha.3
Super User

Hi,

I see no problem - same, as with any other dual opamp.

Just they are not "fast" as comparator, 0,7V/us slew, about 4us switching time ; if this is enough for you , then ok.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
AScha.3
Super User

Hi,

I see no problem - same, as with any other dual opamp.

Just they are not "fast" as comparator, 0,7V/us slew, about 4us switching time ; if this is enough for you , then ok.

If you feel a post has answered your question, please click "Accept as Solution".

Thank you!

I just wanted to confirm as I can see that some manufacturers spec both for and against for some of their amplifiers. 

best regards,

Mg