Associate II
Apr 8, 2022 2:49 PM UTC
Question
Problems with time server and STM32CubeIDE debugging
- 3 replies
- 2232 views
I was trying to use the time server for a project on STM32WB55. I tried to use it in an empty project. When I tried to debug, this window pops up:
The curious part of the problem is that this error seems to happen with the time cluster only: using another cluster such as the on/off one doesn't create any problem.
I will attach to this message the .ioc that I am using: I did not modify the STM32CubeMX output.
What can I do?
Thanks in advance.
P.S. Another thing I tried to do was removing and putting back single lines of code in order to understand which part of the program caused the problem. I figured out that the whole thing runs without encountering this specific problem when I remove this line:
/* file: app_zigbee.c */
zigbee_app_info.time_server_1 = ZbZclTimeServerAlloc(zigbee_app_info.zb, SW1_ENDPOINT, &TimeServerCallbacks_1, NULL);