Hi Lucas,Perfectly agree with this:>Unfortunately it seems that there is no possibility to completely prevent the stack from using malloc. Functions like ZbStartup(), ZbZclClusterAlloc() internally use it. As a consequence, a malloc-free implementati...
Hi Lukas,Thanks to have pointed us that AN5500 contains a reference to non existing ZbMemConfig(). It does not exist (anymore?) indeed.- Has anyone managed to use the Zigbee stack with pre-allocated memory and prevent the stack from using malloc? I ...
Hi Maxim, I would be very happy to help you but I am not sure I will with this answer: not reproducing the error since not exactly the same setup at my side, hence only "ideas" (that you certainly already had in this message. It is very easy to have ...
Hi Maxim,Those 3 functions (ZbShutdown,ZbStatePause,ZbStateResume) are not directly related to reducing energy consumption. They are targeting concurrent mode applications (static or dynamic BLE + Zigbee for example). Pause and Resume are then necess...
Hi Maxim, Previously to the initial setup step, the SED will desperately search for a coordinator, hence, with the application Zigbee_OnOff_Client_SED, you need to provide also a coordinator, else you will stay in the "previous to setup commissioning...