cancel
Showing results for 
Search instead for 
Did you mean: 

System View Description file for STM32F105

Adam Hamilton
Associate III

The System View Description (SVD) file for the STM32F1 series does not contain a file for the STM32F105. Because the product selector lumps the 105/107 into the same view, can I assume that the STM32F107.svd file can be used for the STM32F105?

Also, does ST plan on releasing these on their GitHub repositories

Thanks

3 REPLIES 3
Uwe Bonnes
Principal II

F105 and F107 have the same MCUID, so they are the same chip.

Imen GH
ST Employee

​Hello,

I confirm that the same SVD file applies for STM32F105/107 as they have the same IPs characteristics (according to datasheet).

I have raised your feedback internally to take into consideration. A request has been reported of the SVD files to be placed on ST web site.

Regards,

Imen

Thanks Imen, much appreciated.

I look forward to them being made available because at the moment, the SVD files are hosted on a third party repo but I am never sure if they are kept up to date.

Kind regards

Adam