2020-10-06 01:27 AM
Hi,
STM32F103CBT6 controller is used as "ST_link controller" in NUCLEO-F746ZG Nucleo board.
I'm looking for NUCLEO-F746ZG board's ST-link USB bootloader and programming file (.out file) for STM32F103CBT6 controller. Can someone send me link/path for ST-link's (STM32F103CBT6 controller) USB bootloader and programming file (.out file)
I'm making ST-link board design using STM32F103CBT6 controller. So, I'm looking for above mentioned file
Solved! Go to Solution.
2020-10-09 07:43 AM
If both channels really need to be transmitted to the host, ST-LINK/V2-1 might be a good choice. It is part of almost all NUCLEO-64 and can be broken from the target board. It offers RXD/TXD for the UART channel and SWD for the debug channel. You will find an overview of the available NUCLEO here.
The only downside: it's just a board and comes without a case. There are also some guys who use this exact approach, e.g.
https://jeelabs.org/book/1547a/
Does it answer your question?
/Peter
2020-10-09 03:20 AM
No programming file is available and you are not authorized to do so. Please read the Open Platform license agreement.
Maybe the ready to buy ST-LINK/V2 is an option for you?
Regards
/Peter
2020-10-09 03:43 AM
Thanks Peter,
I thought Nucleo board's ST-link design is open source code.
In Nucleo, Both ST-link and "UART to USB" integrated in same/single USB connector. If I use ST-LINK/V2 as external programmer device, then how to combine "UART to USB" and external ST-link programming cable's USB connectivity on the same USB connector interface?
2020-10-09 04:29 AM
Hi, @S.Kamath,
It's not really difficult to combine multiple data streams on one USB port, as this is what USB was designed for. The STM32F103 at the ST-LINK/V2 just merges the SWD stream and the UART stream.
BTW: thanks to the more powerful STM32F7, the ST-LINK/V3 merges even more data into the data stream: SPI, I2C, CAN or GPIOs.
Regards
/Peter
2020-10-09 07:08 AM
Thanks for Peter for prompt response.
If I use ST-LINK/V2 as external programmer device, then how to combine "UART to USB" and external ST-link programming cable's USB connectivity on the same USB connector interface?
I do agree that we can manage entire solution by using STM32F103. But, this solution requires firmware development. I'm looking for solution without using firmware development
2020-10-09 07:43 AM
If both channels really need to be transmitted to the host, ST-LINK/V2-1 might be a good choice. It is part of almost all NUCLEO-64 and can be broken from the target board. It offers RXD/TXD for the UART channel and SWD for the debug channel. You will find an overview of the available NUCLEO here.
The only downside: it's just a board and comes without a case. There are also some guys who use this exact approach, e.g.
https://jeelabs.org/book/1547a/
Does it answer your question?
/Peter
2020-10-09 07:45 AM
Thanks for suggestions..!! I was thinking same approach before I ask my previous questions 🙂