cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot access STM32F103CBT6 again after downloading program created by latest CubeMX 6.10.0.

MNapi
Senior III

I created new program using latest CubeMX 6.10.0, I use Keil. I upload without any problems.

I use ST Link v3 connected to PA13 (SWDIO) , PA14 (SWCLK)

The program is running but when I try to connect again it says STM32 not found.

I cannot debug, I cannot download again.

There is no extra code, only plain code created by CubeMX, all pins are not enabled, nothing.

Still the same problem.

 

I connect pin BOOT0 to 3.3V and suddenly I can access the chip again and upload program.

 

When I use program created by older CubeMX, I do not have this problem.

Has anybody seen something like this ? There must be something with the code generated by latest CubeMX

I haven't check other chips I have noticed this only with STM32F103CBT6. Other might be affected too.

 

 

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Semer CHERNI
ST Employee

Hello

After analyzing the generated code, I found that the void HAL_MspInit(void) contains a call for a macro which set the GPIO debug pins according to the setting done in the CubeMX :

SemerCHERNI_0-1704809251554.png

The screenshot shows the default stat which will make the CubeMX insert the following code in HAL_MspInit(void) which disable the SW debug

  /** DISABLE: JTAG-DP Disabled and SW-DP Disabled
  */
  __HAL_AFIO_REMAP_SWJ_DISABLE();

 To be able to make it debug correctly, you need to explicitly set the Debug settings in CubeMX (Case of SW with ST-Link)

SemerCHERNI_1-1704811712250.png

  /** NOJTAG: JTAG-DP Disabled and SW-DP Enabled
  */
  __HAL_AFIO_REMAP_SWJ_NOJTAG();

 

KR,
Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

12 REPLIES 12
TDK
Super User

Probably the SWDIO/SWCLK pins are being re-assigned. Attach the IOC or code. Do you have "set unused pins as analog" or similar setting enabled?

> all pins are not enabled, nothing.

Set SWD pins to SWD functions to avoid them getting messed with.

If you feel a post has answered your question, please click "Accept as Solution".

Nothing is messed up. Read carefully my original post.

I can set pins to anything I want or not set to anything and the problem stays on.

setting pins to analog or not setting to anything else does not have influance/change on the problem.

See original post I do not have the problem with older version of CubeMX

SWD pins are set to SWD and nothing is messed up.

TDK
Super User

Certainly, you can diff the code and see what is changed.

If you feel a post has answered your question, please click "Accept as Solution".

>>I haven't check other chips I have noticed this only with STM32F103CBT6. Other might be affected too.

The F1 does have it's own relatively unique method for disabling the JTAG-DP pins in several stages.

Likely a change in a default setting deep in the project meta data.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
oeliks
Senior

Noticed this also. On clone/fake that I dont use - I though it was cheap genuine chip (when I bought it several years back) but starting wondering when it behavined funny in some situations.

 

I tried to upload some old code that certainly was working (on genuine mcu's and this clone also).

 

Is it genuine part from official reseller?

From the first look it really seems to be bricked ;)

It is genuine from Mouser. But I got also a whole bunch from Aliexpress they are less than $1 compared to $10 on mouser. No difference. The problem is always there when I use latest CubeMX

We need ST tech support to look at this.

But I have just tried different chip (STM32H7A3ZIT6) on latest CubeMX (6.10.0) and I did not have this problem.

 

 

Diff the code between working and non-working forks.

Grep/Search for code streams like these

  /* Remap SPI1 pins and disable JTAG */
  LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_AFIO);
  LL_GPIO_AF_Remap_SWJ_NOJTAG();
  while((AFIO->MAPR & AFIO_MAPR_SWJ_CFG_JTAGDISABLE) != AFIO_MAPR_SWJ_CFG_JTAGDISABLE);

Basically the AFIO unit and the SWJ settings

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

I can spend a day comparing the code of working and not working. The point is that latest CubeMX (6.10.0) is generating the not working code and ST has to fix it.

 

I do not know if it is only STM32F103CBT6 or whole STM32F1 family or more.

>>ST has to fix it

Sure, and I've flagged the post for review, but if you identify the code that's compiled and running that's disabling the pin function, or the settings within the tools that's causing them to build this way it will get fixed quicker. But it's unlikely to done in a few days, and definitely not at the weekend.

A Find-in-File should take less than a minute. "_SWJ_"

The code flow from Reset_Handler(),  SystemInit(), HAL_Init() shouldn't be that difficult to pin down.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..