Associate
Feb 26, 2020 12:41 PM UTC
Question
Configuring STM32F746GDISCOVERY TouchGFX graphic application via STM32CUBEMX and STM32CubeIDE
- 11 replies
- 3474 views
I have just spent two days configuring STM32F746GDISCOVERY graphic application via CUBEMX an finally get it work. So I'm sharing my steps.
It is written for dummies like me =)
Many thanks to Martin Kjeldsen for background information.
There are DOCx, RARed images, ioc file and whole project in the attachmments.
Edit: I should have mentioned that all the code added to main.c and other settings are from project generated by TouchGFX Designer.
Edit2: QUAD SPI is not configured corretly, here is the roght configuration in the video: