cancel
Showing results for 
Search instead for 
Did you mean: 

Can Source code be released for 'Guifw-STM32F4xx-Nucleo.bin' ?

EZamo.1
Associate III

I'm interested in using the Nucleo StmH7 with the L6474 X-NUCLEO-IHM01A1 board.

However I'd like to run STSW-SPIN002 to communicate with it, but that expects to talk to the NUCLEO-F401RE... so I need the protocol that's implemented in order to port to the NUCLEO-H743ZI.

Is it possible to get the source code for Guifw-STM32F4xx-Nucleo.bin?

2 REPLIES 2
Martin KJELDSEN
Chief III

It doesn't sound like it's TouchGFX running on that board, so its definitely not something we've done here at the office. I'll try asking around.

/Martin

If the source code that runs on the Nucleo cannot be open-sourced (to be ported to the Nucleo H743ZI) , what about source code for the other side.. the PC software STSW-SPIN002 that talks to it?

If neither, how difficult would implementing the motor movement protocol based on just analyzing the serial traffic between the PC SPIN and the Nucleo F401RE?