cancel
Showing results for 
Search instead for 
Did you mean: 

Problem generating SW4STM32 Project on Windows 10

SJaco.1
Associate

Hi,

I use CubeMX to configure STM32 controllers (mostly STM32F746ZG for testing on a Nucleo-144 board, but also tried with other boards and single MCUs).

Since I moved to Windows 10 64Bit, the generation of SW4STM32 projects does not work properly anymore (both with newly created and old IOC files). The following problems appear:

- The MCU (to be configured in SW4STM32 under Project Properties -> C/C++ Build -> Settings -> MCU Settings) is not configured. This does not allow the selection of FP hardware.

- The linker script is not created / linked to the project (probably a consequence of the first point).

I use the following program versions (latest updates):

- CubeMX v5.5

- CubeF7 Package v1.15.0

- SW4STM32 v2.9

I have also tried a complete new installation and the usage of older versions. The problem remains the same. Also, the generation for MDK-ARMv5 shows a similar effect with the additional error message:

0690X00000Bw0n3QAB.jpg

Does anyone have an idea what the problem might be / how to fix it?

Thanks for your help

Sven

1 REPLY 1
dbgarasiya
Senior II

you should try stm32cubeide

https://www.st.com/en/development-tools/stm32cubeide.html

go above link and install , easy to wok