Associate II
Nov 13, 2019 5:17 AM UTC
Solved
32F746 USART DMA with STemWin not working.
- 9 replies
- 3344 views
I'm working on STM32F746 discovery wtih STemWin(firmwere F7 1.15). I'm tested on both UART1 and UART6.
It's work fine without DMA and it's also worked with interrupt too.
When i try to run with DMA. Hardware not even send an output data(I'm checked with my oscilloscopes). And huart keep busy all the time.
So i give up trying on STM32F746 discovery. And tested on STM32F746 Nucleo board. I'm setup with cudeMX. And enabled only UART2 and UART3 with DMA and global interrupt. Than i'm found the problems UART3 DMA not wotking but UART2 DMA work fine. And than i try UART2-3 without DMA , Only interrupt. And It's works.
I'm tried to result this problem for 2 days now. And i have no clue what's wrong with it. Please help me.