cancel
Showing results for 
Search instead for 
Did you mean: 

L9942 not working properly accoding to the sample

JHeo.1
Associate

Hello 

I'm a newer about  stepping motor IC L9942

I compsed of  L9942 Climate control Unit in HVAC .

Some devices have no problem when they are controlled by a program.

A specific device rotates discontinuously when it rotates.

I am looking for the cause of whether this is a program error or a circuit problem.

I wonder if the EVA board is made up of 6.8Kohm resistor (R8) for Rref, and what is the effect of lowering the resistance value?0690X000009Zdj3QAC.png

0 REPLIES 0