cancel
Showing results for 
Search instead for 
Did you mean: 

Does STM32F429 support SPI RGB Serial Interface?

changli
Associate II
Posted on December 30, 2013 at 14:52

I found a LCD with OTA5182A driver in SPI & RGB interface. However its RGB is serial RGB not parallel RGB in STM32F429. Is there a way to allow the LCD controller to work with STM32F429 inside lcd display?

#interface-anything-to-anything
3 REPLIES 3
Andrew Neil
Evangelist III
Posted on January 01, 2014 at 11:18

So it goes back to just a standard interfacing problem:  

http://www.8052.com/forum/read/160143

Andrew Neil
Evangelist III
Posted on December 30, 2013 at 19:51

The STM32's SPI neither knows nor cares anything about the meaning of the data it transfers - so you can program it to carry whatever data you like!

changli
Associate II
Posted on December 31, 2013 at 16:56

The problem is that serial RGB has only 8-bit data line, the parallel has 3*8 data lines. The LCD control will be different. The Discovery board connected 24 data lines from LCD display. And there is no frame buffer (RAM) in serial RGB LCD display.