Skip to main content
June 1, 2024
Question

Touchgfx; How to Play video from SD Card?

  • June 1, 2024
  • 2 replies
  • 2108 views

Hello everyone 

Is there any example that I can use to read avi file from SD- CARD and pass it to TouchGFX 

Function?

Now I can play video from RAM at address 0xD0780000 for instance, 

This is TouchGFX Function but I don't know how to use it?

  • Any help,  I would appreciate :folded_hands: 

class MyReader : public touchgfx::VideoDataReader
{
public:
MyReader() : position(0) { }
virtual uint32_t getDataLength() { return video_len; }
virtual void seek(uint32_t pos) { position = pos; }
virtual bool readData(void* dst, uint32_t bytes)
{
memcpy(dst, &video_data[position], bytes);
position += bytes;
return true;
}
private:
uint32_t position;
} myReader;

 

video.setVideoData(myReader);

 

https://support.touchgfx.com/docs/development/touchgfx-hal-development/scenarios/scenarios-video-decoding#filereader-interface 

2 replies

MM..1
Chief III
June 1, 2024

As described in docs you can replace reader memory with any other reader, but most optimal is memory mapped direct access any other is slower . When you choice , simply replace

 

memcpy(dst, &video_data[position], bytes);

 

 with some fopen fseek ...

June 2, 2024

Thanks for your reply 

But how about ,seek, and read data and length ?

When I use this comment always get error

video.setVideoData(myReader)

It is better to send my code maybe you can help me better :) 

ST Employee
June 4, 2024

Hello @unknown ,

First welcome to the TouchGFX community. When you add code to your post, please format your code for better readability by clicking on this icon: 

LouisB_0-1717494424676.png

Can you add some details ? What error did you get ?

Regards,

Louis BOUDOST Software Engineer | TouchGFX
June 5, 2024

Hello
thanks for your response
Yes, you are right
I present the program files to you and have taken a short video of the debugging moment, which I hope will solve the problem by looking at it. I wish there were an example of a project to learn from

This is the link to the video  it's a zip file

 

#define BUFFER_SIZE ((uint32_t)4500)
 uint32_t video_len;
 uint32_t video_data[BUFFER_SIZE];


class MyReader : public touchgfx::VideoDataReader
{
public:
 MyReader() : position(0) {}
		virtual uint32_t getDataLength() { return video_len; }

 virtual void seek(uint32_t pos) { position = pos; }
 virtual bool readData(void* dst, uint32_t bytes)
 {
			cunter=position; // I added 
 memcpy(dst, &video_data[position], bytes);
 position += bytes;
 return true;
 }

 private:
 uint32_t position;
} myReader;


void VideoScreenView::playFunc()
	
{
	video1.setVideoData(myReader);
 video1.play();
	
}





 if (!(attributes & 0x18) && (status == FX_SUCCESS))
 {
 
 /* Try to open the file. */
 status = fx_file_open(&sdio_disk, &my_file, PicFolderName.PicImage, FX_OPEN_FOR_READ);
	 status = fx_directory_information_get(&sdio_disk,PicFolderName.PicImage, 
 &attributes, &size,&year, &month, &day,&hour, &minute, &second);
		
	 video_len =size; //read the file size

 /* Read the entire file. */
 if (status == FX_SUCCESS)
 {

 while(1) /* EOF or Error */
 {
 /* Seek start of File */
 	fx_file_seek(&my_file,cunter);
 /* Read the file in blocks */
 status = fx_file_read(&my_file, video_data, sizeof(video_data),
 		 &byteswritten22);
}

//and stock here 

const uint8_t* SoftwareMJPEGDecoder::readData(uint32_t offset, uint32_t length)
{
 if (reader != 0)
 {
 if (length > aviBufferLength)
 {
 lastError = AVI_ERROR_FILE_BUFFER_TO_SMALL;
 assert(!"Buffer to small");
 }

 reader->seek(offset);
 if (!reader->readData(aviBuffer, length))
 {
 lastError = AVI_ERROR_EOF_REACHED;
 }

 aviBufferStartOffset = offset;
 return aviBuffer;
 }

 return movieData + offset;
}