2017-09-22 05:25 AM
Dear all,
I'm having a problem creating a arbitrary waveform using timer 1, MCU STM32L476RG. I use STM32CubeMX (4.21.0) to generate all initialization code after which I try to start a DMA transfer from memory to the timer 1 peripheral. I'm partly successful doing this.
I created a array of 6 words for two waveform patterns to be send to TIM1 channel 1 (TIM1_ARR, TIM1_RCR, TIM1_CCR1) This is how the basics look
uint32_t aSRC_Buffer[6] = { 100, 2, 15, 100, 8, 50 }; /// ARR, RCR, CCR1 x 2
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1) ;
HAL_TIM_DMABurst_WriteStart(&htim1, TIM_DMABASE_ARR, TIM_DMA_UPDATE, (uint32_t*) aSRC_Buffer, TIM_DMABURSTLENGTH_3TRANSFERS);With this code only the first pattern is generated. changing TIM_DMABURSTLENGTH_3TRANSFERS to TIM_DMABURSTLENGTH_6TRANSFERS does not work either (seems right if my assumption is correct, see below).
I don't understand the relation between the complete DMA buffer size (mem) and the TIM registers update. Right now I assume that setting TIM_DMABURSTLENGTH_3TRANSFERS means the three TIM registers starting at ARR are updated. But how do I set the total buffer size to use. I have tried to set DMA1_Channel6->CNDTR = 6; in the HAL_TIM_Base_MspInit routine but that didn't help either. I'm lost.... Is there anyone that can explain to me what I am missing here.
some cubemx settings are :
DMA1 -> DMA1 channel 6 -> memory to peripheral -> priority high
Mode normal Increment address -> memory only
Data width word
Partly generated code is
if(htim_base->Instance==TIM1)
{/* Peripheral clock enable */
__HAL_RCC_TIM1_CLK_ENABLE(); hdma_tim1_up.Instance = DMA1_Channel6; hdma_tim1_up.Init.Request = DMA_REQUEST_7; hdma_tim1_up.Init.Direction = DMA_MEMORY_TO_PERIPH; hdma_tim1_up.Init.PeriphInc = DMA_PINC_DISABLE; hdma_tim1_up.Init.MemInc = DMA_MINC_ENABLE; hdma_tim1_up.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD; hdma_tim1_up.Init.MemDataAlignment = DMA_MDATAALIGN_WORD; hdma_tim1_up.Init.Mode = DMA_NORMAL; hdma_tim1_up.Init.Priority = DMA_PRIORITY_HIGH; if (HAL_DMA_Init(&hdma_tim1_up) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); } __HAL_LINKDMA(htim_base,hdma[TIM_DMA_ID_UPDATE],hdma_tim1_up);/* TIM1 interrupt Init */
HAL_NVIC_SetPriority(TIM1_UP_TIM16_IRQn, 0, 0); HAL_NVIC_EnableIRQ(TIM1_UP_TIM16_IRQn);}
Thanks in advance,
Wim
2017-09-23 06:25 PM
I found the same issue.
I traced it to the
HAL_TIM_DMABurst_WriteStart method.
If you used AN4776:General-purpose timer cookbook, Section 5as a reference, the sample code (using LL)
for a burst of 3 sets of 3 registers;
The sample sets DMA CNDTR to 9 words
/* Write to DMA1 Channel5 number of data’s register */
DMA1_Channel5->CNDTR = 9;�?�?�?�?
The sample s
ets
each burst 3 words/* Select the DMA base register and DMA burst length */
TIM1->DCR = TIM_DMABase_ARR | TIM_DMABurstLength_3Transfers;�?�?�?�?
InHAL, youstart a burst transfer with;
HAL_TIM_DMABurst_WriteStart(TIM_HandleTypeDef *htim,
uint32_t BurstBaseAddress,
uint32_t BurstRequestSrc,
uint32_t *BurstBuffer,
uint32_t BurstLength)�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
In older HAL versions, this method put burstlength into both CNDTR and DCR;
HAL_DMA_Start_IT(htim->hdma[TIM_DMA_ID_CC1], (uint32_t)BurstBuffer, (uint32_t)&htim->Instance->DMAR, BurstBuffer);
htim->Instance->DCR = BurstBaseAddress | BurstLength;�?�?�?�?�?�?
I wrote a patch when i had this issue.
But I just looked in new HAL that came with F3 FW1.9.0 and they seem to have fixed this;
HAL_TIM_DMABurst_WriteStartcalls a new HAL_TIM_DMABurst_MultiWriteStart
HAL_StatusTypeDef HAL_TIM_DMABurst_WriteStart(TIM_HandleTypeDef *htim,
uint32_t BurstBaseAddress,
uint32_t BurstRequestSrc,
uint32_t *BurstBuffer,
uint32_t BurstLength)
{
return HAL_TIM_DMABurst_MultiWriteStart(htim, BurstBaseAddress, BurstRequestSrc, BurstBuffer, BurstLength, ((BurstLength) >> 8U) + 1U);
}
HAL_TIM_DMABurst_MultiWriteStart(TIM_HandleTypeDef *htim,
uint32_t BurstBaseAddress,
uint32_t BurstRequestSrc,
uint32_t* BurstBuffer,
uint32_t BurstLength,
uint32_t DataLength)�?�?�?�?�?�?
{
.
.
.
HAL_DMA_Start_IT(htim->hdma[TIM_DMA_ID_UPDATE], (uint32_t)BurstBuffer, (uint32_t)&htim->Instance->DMAR, DataLength);
.
.
.
htim->Instance->DCR = BurstBaseAddress | BurstLength;
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?.
.
.
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
Try updating your HAL FW version. In your case you should call;
#define buffersize 6
uint32_t aSRC_Buffer[buffersize ] = { 100, 2, 15, 100, 8, 50 }; /// ARR, RCR, CCR1 x 2
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1) ;
HAL_TIM_DMABurst_MultiWriteStart(&htim1,
TIM_DMABASE_ARR,
TIM_DMA_UPDATE,
(uint32_t*)aSRC_Buffer,
TIM_DMABURSTLENGTH_3TRANSFERS,
buffersize );�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
2017-09-25 05:03 AM
I Agree,
Again thanks!
2017-09-25 06:13 AM
Hi John,
Thank you very much for explaining the ins and outs. You gave me the assurance that I'm not crazy -:) It seems that version 1.0.9 is only supporting the STM32Fxx series for burst multi write and read. Anyway , the Lxx devices are not supported yet. I think I will just have to create a patch to get thing going.
Thanks.
2017-09-25 06:52 AM
It should be pretty easy to take the MultiWriteStart from the current F3 HAL fw and adapt it to your Lxx model.
2017-09-25 06:54 AM
Hopefully STM is listening and get this issue fixed in all the HAL versions soon.
2018-02-12 02:35 PM
I'm having the same issue. I'm using an L4 series part and I don't see the multiWriteStart in the HAL. Where and how in the code did you put in the patch to incorporate the dataLength ?
Thanks!
2018-02-28 01:31 AM
Hello!
You can open ~/STM32Cube/Repository/STM32Cube_FW_F3_V1.9.0/Drivers/STM32F3xx_HAL_Driver/Src/stm32f3_hal_tim.cAnd simple copy HAL_TIM_Burst_MultiWriteStart.
Different between
HAL_TIM_Burst_MultiWriteStart
andHAL_TIM_Burst_WriteStart
is that:HAL_DMA_Start_IT(...,...,...., ((BurstLength) >> 😎 +1) //HAL_TIM_Burst_WriteStart
HAL_DMA_Start_IT(...,...,...., DataLength) // HAL_TIM_Burst_MultiWriteStart
2018-03-02 11:07 AM
No its wrong, BurstLength is not DataLength, copy HAL_TIM_DMABurst_MultiWriteStart from HAL_F3 into your USER SECTION CODE (to preserve HAL sources), use it and remove it when HAL_L4 will be upgraded.
2018-03-04 10:01 PM
Where was I wrote, '
BurstLength is DataLength'?
I wrote that the argument((BurstLength) >> 😎 +1 (not BurstLength!) have used for
HAL_DMA_Start_IT function.
Configuration of DMA Burst Mode is not changed!
htim->Instance->DCR = BurstBaseAddress | BurstLength; // HAL_TIM_DMABurst_WriteStarthtim->Instance->DCR = BurstBaseAddress | BurstLength; // HAL_TIM_DMABurst_MultiWriteStart