2023-09-24 3:53 AM
Hi everyone,
I am trying to generate an arbitrary PWM waveform using DMA burst write according to AN4776. It works in principle, except of one thing: If i want to have more than one pulse with a specifig period/pulse setting, the RCR should be used. However, no matter what I write to RCR one one pulse with the corresponding settings is generated.
I wrote a short test code.
The burst write data is:
const uint16_t curve_test[4] = {0x50F,0x50F,0xFE,0x288}; // PSC,ARR,RCR,CCR1
Pulse pattern is startet with:
htim1.hdma[TIM_DMA_ID_CC1]->Instance->CR |= DMA_SxCR_MINC;
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1);
HAL_TIM_DMABurst_MultiWriteStart(&htim1,TIM_DMABASE_PSC,TIM_DMA_CC1,(uint32_t *) &curve_test[0],TIM_DMABURSTLENGTH_4TRANSFERS,(uint32_t) 4);
and stopped with:
void HAL_TIM_PWM_PulseFinishedCallback(TIM_HandleTypeDef *htim)
{
BaseType_t xHigherPriorityTaskWoken;
xHigherPriorityTaskWoken = pdFALSE;
HAL_TIM_PWM_Stop_DMA(htim,TIM_CHANNEL_1);
HAL_TIM_DMABurst_WriteStop(htim,TIM_DMA_CC1);
xSemaphoreGiveFromISR(xSemaphoreStepperCmplt,&xHigherPriorityTaskWoken);
portYIELD_FROM_ISR(xHigherPriorityTaskWoken);
}
Using this code I only get one pulse per call. Does anyome has a hint what I might do wrong?
BR
Daniel
2023-09-24 10:13 PM
Which STM32?
I am not interested in discovering how various Cube/HAL contraptions are supposed to be used, but I suspect some of the functions you are calling in the callback actively disable the timer. Place a breakpoint at the beginning of that function and observe both output and the involved peripherals' registers.
JW
2023-09-25 10:43 AM
I have founde the mistake. The problem was that the burst transfer and DMA transfer was related to Capture Compare and not to update event. I had to configure the DMA channel to "TIM1_UP" and to call the burst transfer by
HAL_TIM_DMABurst_MultiWriteStart(&htim1,TIM_DMABASE_PSC,TIM_DMA_UPDATE,(uint32_t *) &curve_data[0],TIM_DMABURSTLENGTH_4TRANSFERS,(uint32_t) puls_cnt);.
The related callback then is:
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)