cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 PLL minimum input frequency

Uwe Bonnes
Principal II
Posted on October 18, 2017 at 11:10

Hello,

STM32H743 datasheet Rev. 2  in chapter 6.3.10 PLL characteristics tells 2 MHz minimum PLL input clock (f (PLL_IN)). Reference manual RM0433 Rev 3 in chapter 8.5.5 'PLL description' tells about a low frequency VCO(VCOL) for input frequencies 1 to 2 MHz. Pleas resolve this inconsistancy.

1 REPLY 1
Nesrine M_O
Lead II
Posted on October 18, 2017 at 15:49

Hi

Bonnes.Uwe

,

You are right. Thank you for bringing this issue to our attention, in fact we have to add a dedicated table for theA low-frequency VCO.

It is noted and will be fixed in coming release of the datasheet.

-Nesrine-