cancel
Showing results for 
Search instead for 
Did you mean: 

stm32 lora

Posted on May 08, 2017 at 08:48

Hi. I have to study the lora world with a stm32 microcontroller.

For me it is the first approach. Can someone suggest me witch stm32 demo board is the most easy to use in order to learn how lora works?

Can someone suggest me a tutorial?

I need to use lora as sensoristic application.
7 REPLIES 7
Khouloud GARSI
Lead II
Posted on May 08, 2017 at 11:10

Hi

Gottardello.Deni

‌,

The application note

https://my.st.com/content/ccc/resource/technical/document/application_note/group0/db/8c/4f/5a/95/9e/40/69/DM00346311/files/DM00346pdf/jcr:content/translations/en.DM00346pdf

may also help you.

Khouloud.

Posted on May 08, 2017 at 14:53

I'd recommend the 

B-L072Z-LRWAN1, it is a DISCO board which includes and ST-LINK debugger and the LoRa via a Murata part including an STM32L0 device and the SX1276 radio.

The USI module is a closed source solution, and the AT modem firmware lacks refinement, the L0 part has significantly less memory, and it uses the older SX1272 radio. I would avoid.

The NUCLEO and SX127x radio pairings work well.

The 

I-CUBE-LRWAN works relatively seamlessly across a number of board combinations, although the code has some significant deficiencies.

I'm using LoRa as a point-to-point radio link.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on May 30, 2017 at 16:12

Many thanks.

Posted on May 30, 2017 at 16:38

https://community.st.com/0D50X00009bMM5DSAW

 
LMI2
Lead
Posted on May 30, 2017 at 21:00

Who sells the

B-L072Z-LRWAN1

, both Digikey and Mouser have zero stock.
Posted on May 30, 2017 at 21:36

They had stock, and sold it. You'll have to back order and wait for deliveries.

If August isn't appealing, then consider your other options

Bunch of stock of the P-NUCLEO-LRWAN1 combo board. Qty 222 as I type

http://www.mouser.com/new/stmicroelectronics/stm-p-nucleo-lrwan1/

 
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Artur IWANICKI
ST Employee
Posted on May 24, 2018 at 07:49

Hello,

I would like to recommend to you one of our on-line courses dedicated to LoRa.

It is a recording of our LoRa workshop session from last year.

Session is free and it requires a free registration.

More information and access link you can find

http://www.st.com/content/st_com/en/about/events/events.html/lora-mooc-connect-your-long-range-network-to-the-cloud.html

.

Best Regards,

Artur