Hello, I would recommend to you an example within STM32F4 Cube library related to STM32F4xG-EVAL board with similar MCU as a base.
example can be found within the library here:
.\STM32Cube_FW_F4_V1.27.1\Projects\STM324xG_EVAL\Applications\FreeRTOS\Fr...
Hello,
There is DAC in this MCU. The issue you are observing is related to the ICache activity on read-only part of the memory (package information). To solve the issue you can either disable ICache or disable cacheability of this region. Please have...
Hello,
This pin is available only within packages with an external SMPS supply option (having P or PTR suffix in the marking, i.e. STM32L412RBT6P) and it is connected directly to Vcore power line (Core, Memories and Digital peripherals supply).
Vdd12...
Hello,It will work. In case ADC data will not be available function will return HAL_TIMEOUT (numerical 3). In case of data presence HAL_OK (numerical 0).But calling this function one by one with 0 timeout will cost your application quite a lot of tim...
Hello,In case you are using CMSIS_OS you can refer to example code within "FreeRTOS on STM32 v2" MOOC:https://www.st.com/content/st_com/en/support/learning/stm32-education/stm32-moocs/freertos-common-microcontroller-software-interface-standard-osv2.h...