cancel
Showing results for 
Search instead for 
Did you mean: 

Compile time is taking forever

mbmail4
Associate II
Posted on December 18, 2017 at 20:18

Hi Everyone.

I recently updated my SW4STM32 IDE when prompted to do so from a pop up, and I'm now seeing its taking forever to compile a project. For example I cleaned one of my

mailto:STM#@F0

Adafruit LCD shield demo programs and then rebuilt it with the following stats finally displayed via the console view.

06:07:06 Build Finished (took 1m:46s.283ms), this is forever?

It was going through building each file one by one taking at least a second or so on each file. Is this something someone else is experiencing, can I fix this somehow?

EDIT: Also making a trivial code change produced this.

06:20:51 Build Finished (took 4s.363ms)

Thanks

mb

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Alexandre Meyer
Associate II
Posted on May 24, 2018 at 06:10

Hi

B.M.002

‌,

What was the code change you made to speed up compilation ?

My full project is taking 15 minutes to compile for no special reason.

Thanks a lot

Alex