cancel
Showing results for 
Search instead for 
Did you mean: 

Max/min application speed cannot read

freppa
Associate II
Posted on June 18, 2018 at 12:35

Referring to UM1052, chapter 14.

It says that register s 0x3F and 0x40 are available to read using the get register command frame over UART. 

I have most of the other registers up and running, so the problem is not with UART com.

I get the response bach from the motor control board with error code 0x03 'Read not allowed. The value cannot be read'.

Anyone having the same problem. I see where in the code to fix this, but I guess it should be reported as a bug.

Fredrik

#uilibrary #uart #st-mcp
0 REPLIES 0