Max/min application speed cannot read
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-06-18 3:35 AM
Posted on June 18, 2018 at 12:35
Referring to UM1052, chapter 14.
It says that register s 0x3F and 0x40 are available to read using the get register command frame over UART.
I have most of the other registers up and running, so the problem is not with UART com.
I get the response bach from the motor control board with error code 0x03 'Read not allowed. The value cannot be read'.
Anyone having the same problem. I see where in the code to fix this, but I guess it should be reported as a bug.
Fredrik
#uilibrary #uart #st-mcp
Labels:
- Labels:
-
Motor Control Hardware
-
UART-USART
0 REPLIES 0