2018-02-12 03:33 AM
Posted on February 12, 2018 at 12:33
Hi,
I got my STEVAL-IDB007V1M with the SPBTLE-1' (based on BlueNRG-1 and installed the STSW-BLUENRG1-DK (v2.6.0). With the help of Antonio (
https://community.st.com/0D50X00009XkWquSAF
) I know, the STEVAL-IDB007V1M works as it should.
I installed Atollic TrueSTUDIO for STM32 9.0.0, I imported the BLE_SensorDemo project as described in 'SensorDemo_BlueMS_main.c File Reference'. I can build the project - when I flash the Release.hex file to the BlueNRG-1 with the 'BlueNRG-1 Flasher' nothing happens on the BlueNRG-1.
Same with Micro_Hello_World
What's wrong?
I set the HS_SPEED_XTAL=HS_SPEED_XTAL_32MHZ in BLE_SensorDemo and I already switched the optimization level to -O0 in the compiler settings of the projects.
TIA, best regards
Wolfgang
2018-02-18 02:17 PM
Hi all
I have the same problem as Wolfgang. I compiled BLE_Beacon example with newest TrueStudio under Windows 7, under Linux, and I even used my own toolchain, all 3 with no luck whatsoever. I Flashed the binary both using the flasher application provided by ST, and using ST-link via SWD interface. The program crashes with the following stacktrace:
1 HardFault_Handler BlueNRG1_it.c 68 0x10040ac8
2 ?? 0xfffffff9 3 IDD_Initialize_Device_IDs 0x10054df0 4 GAP_Init 0x10043a7c 5 aci_gap_init 0x100434ce 6 Device_Init BLE_Beacon_main.c 75 0x100408e2 7 main BLE_Beacon_main.c 210 0x10040a66 But since BLE stack is provided only in binary, I am unable to investigate what's happening inside. At the same time I was able to successfully run the GPIO/IOToggle example, but as you might expect it does not use the BLE stack. Later on I checked all the BLE examples, and none of them (I mean when compiled with TrueStudio by me) worked.At this point I suspect some misconfiguration in the projects (?) Also, it would be wise to check non-GCC compilers as well, but I have no experience with them. BTW does anybody know what compiler ST uses for the examples bundled in the SW package (I mean those in the 'firmware' directory)?2018-02-19 06:43 AM
I managed to finally run BLE_Beacon but unfortunately I compiled it with my own cross compiler (GCC based). The stacktrace and the error I posted above was due to me using BlueNRG2.ld instead of BlueNRG1.ld during linking. Apparently those 'device_ids' are stored at the very end of flash memory, which in case of BlueNRG2 is slightly bigger. Thus my NRG1 was trying to write onto nonexistent flash. I still don't know why projects compiled with TrueStudio don't work though, and I would love to know this.
2018-02-21 06:29 AM
Hi once again. Piotr Romaniuk, who is also active on this forum suggested that you should add
-mcpu=cortex-m0 to compilation options.
2018-05-11 12:31 PM
Indeed!!!
I spent couple of hours until I found that ISR code contains non Thumb instructions.After specification of sub-architecture compiled code is ok.Regards,
Piotr Romaniuk2018-06-20 07:06 AM
Hi,
I have same problem. I can not build a running bin/hex for STEVAL-IDB007V1M with TrueStudio 9.01.
Is there a solution?
I tried with IAR -> no problem, but I'm looking for a cheap solution :-)
Thanks!
Robert
2018-06-20 11:29 AM
Hi Robert,
please read the thread:
https://community.st.com/0D50X00009Xkht6SAB
Regards,
Piotr Romaniuk