Get ready for the STM32 Summit 2026 | Online, November 3
Join discussions in the Product Forums. Ask questions, learn from your peers, and share insights on ST solutions to accelerate your design journey.
Most recent activity
Hello, I’m having some issues connecting my sensor tile box pro to my pc via a USB cable and with an ST-Link V2. I’ve followed the documentation regarding DFU mode, and the board doesn’t respond to it in STM32 Programmer ( I’ve double checked if its a data cable, and this was confirmed). With the ST-Link, my Device Manager recognizes the debugger, but it has issues communicating/connecting with the board. However, I am able to flash it via Bluetooth. Is there some initialization I missed?
Hello Team, I am using STM32N6,I am using about 50 GPIOs, all for SPI and I2C communications, and the VDD port supplies 200mA, Will the usage of all these pins consume less than 200mA, or do I have to widen the range of VDD? Also, what is the total max current consumed by the STM32N6 during its maximum processing, Please let me know.Thank you.
MCU / setupSTM32F746IGK, VDD = 3.3 V HSE 16 MHz, PLL: M=8, N=200, P=/2 → SYSCLK = 200 MHz (AHB=200, APB1=/4, APB2=/2) Scale 1 + Over-drive, FLASH_LATENCY_6 Already below the 216 MHz maximum Application executes from the ITCM Flash alias (0x002xxxxx; AXI alias 0x080xxxxx) Cortex I-Cache and D-Cache disabled at startup ART accelerator / prefetch enabled in HAL (ART_ACCELERATOR_ENABLE, PREFETCH_ENABLE) Bare metal, 1 ms cyclic scheduler, no RTOS X-CUBE-STL Flash TM every 1 ms: 1 KB window, HW CRC-32 (poly 0x04C11DB7, init 0xFFFFFFFF, word reverse in / reverse out). Expected CRC is a table built offline from the same image (zlib.crc32 / IEEE 802.3).What we see After several hours in RUN (typically ~11–19 h, not at POST), Flash TM returns STL_FAILED (0xD32D) on a 1 KB window. A software CRC of the same window also mismatches, so this is not only the CRC peripheral.On fail we dumped the 1 KB window from the CPU. The dump CRC always equals the TM computed CRC and differs from the programmed im
I have a custom board using an STM32G431RB (LQFP64) that was previously programmable/debuggable without issue. After switching to a new ST-LINK debugger, I started consistently getting:Error: ST-LINK error (DEV_TARGET_HELD_UNDER_RESET)Root cause identified: the board was being powered entirely from the debugger's VDD/VTref pin rather than an independent supply. Powering the board from an external bench supply (debugger providing only SWDIO/SWCLK/GND, not VDD) resolves the connection issue. My working theory is that the ST-LINK's VDD/VTref pin is intended as a voltage sense input, not a real power source, and different probe units/firmware versions apparently have inconsistent (often very limited) current-sourcing capability there — my original debugger happened to supply enough current for this board to stay stable; every replacement unit since (including confirmed-genuine ST-LINK/V2 and V3 probes) could not, leading to what looks like repeated brown-out resets rather than an actual st
Having problem getting STM32C091FCP6 that is new (not otherwise programmed) to respond to STLINK device at power on.Details-Preparing to move a project from STM32C011J6M6 to STM32C091FCP6 to obtain larger pin count and larger memory capacity. On first attempt to attach STLINK V2 device to the target containing a new STM32C091FCP6 (SWDIO, SWCLK and GND to a device on 3.3V power), STLINK not starting as expected (power is being applied before STM32CubeProgrammer is commanded to “Connect.”To rule out PCB layout error on the (new) STM32CX091FCP6-based version of project, I attached another (also new from supplier) MCU to STLINK V2 device attaching only SWDIO, SWCLK and GND to STLINK, applied 3.3V power (all other pins open), and again STLINK not handling “Connect” command as expected. STM32CubeProgrammer is reporting “unable to get core ID” and/or “DFU_TARGET_CMD_ERR.The development environment (STM32CubeProgrammer) and STLINK device firmware are up-to-date.The STM32C091FCP6 devices are fr
Hello everyone,I am working on a custom locker controller board based on the STM8S208CBT6 in the LQFP48 package. I am using the Cosmic C Compiler inside the STVD environment and flashing the MCU via STVP with a standard ST-Link V2 clone.I am experiencing an issue where two specific pins, PD0 (Pin 41) and PC7 (Pin 34), are stuck at a constant logic high level ('1') when configured as standard digital inputs with internal pull-ups (GPIO_MODE_IN_PU_NO_IT), completely ignoring external buttons / shorts to GND. At the same time, six other GPIO pins configured exactly the same way work perfectly fine and detect shorts to GND without any issues.Here is the hardware configuration and what I have observed so far:1. PD0 (Pin 41) is multiplexed with TIM3_CH2, TIM1_BKIN, and CLK_CCO. On this 48-pin package, it is also right next to the SWIM pin (Pin 40). 2. PC7 (Pin 34) is multiplexed with SPI_MISO.3. The board relies on standard UART1 (TX on PA5, RX on PA4) for RS-485 communication, which must re
Hello,I am working on an STM32 USB CDC (Virtual COM Port) device using the STM32 USB Device Library (CubeMX-generated project).My goal is to have the device appear on Windows as a custom COM port name such as:MO3 Device (COMx)However, I want to achieve this without using a custom INF file, since distributing and installing drivers on every PC is not practical for my use case.From my current understanding:The Product String (iProduct) in usbd_desc.c can be modifiedThe Interface String (iInterface) in the CDC descriptor may also influence the displayed nameWindows typically uses usbser.sys and assigns "USB Serial Device (COMx)" by defaultFriendly Name seems to be controlled primarily via INF, not firmwareI have a few specific questions:Is there any reliable way to influence or override the COM port Friendly Name purely from STM32 firmware (USB descriptors), without an INF file?Does modifying iInterface (or using IAD / composite device descriptors) improve the likelihood of Windows using
I am trying to use touchgfx and gfxmmu on H7R7 with a round lcd panel,but failed. So ,Is there a demo of this kind?
I have been reading the discussion here: Understanding the bootloader GO command on the STM32H5 seriesI am trying to understand one point in particular. The discussion describes the problems associated with using the bootloader GO command on STM32H5, and refers to the state of the device and peripherals when the bootloader transfers control to the application. Does the H5 system bootloader GO command actually support transferring execution to an application loaded into SRAM? I ask because the wording left me uncertain about whether the issue being discussed applies to SRAM applications, Flash applications, or both. Perhaps @STea or someone else from ST, could clarify please?
I am currently working with an STM32 MCU and facing an issue while trying to connect the board to my PC using an ST-LINK debugger. The board powers on normally and there does not appear to be any obvious hardware issue, but STM32CubeProgrammer is unable to detect the target device. The connection attempt either fails or reports that no target is found, so I am currently unable to program or debug the MCU.So far, I have checked the basic connections and setup:USB cable and ST-LINK connection Board power supply and voltage SWDIO and SWCLK connections STM32CubeProgrammer installation ST-LINK firmware and connection settingsI am not sure if the problem could be caused by the MCU configuration, SWD interface, boot mode, or some setting that may have been changed in the firmware. I would also like to know if there are any recommended STM32CubeProgrammer options or recovery procedures that should be tried when the target MCU is not detected.Has anyone experienced a similar issue with an STM32
I am trying to build a STM32L0 based low powered project , i am hitting target hold under reset randomly and when i left it power off for few hours its back to working . idk why its happening randomly
I'm trying to get USBX Device MSC to work in Standalone mode (without RTOS). I loosely followed @B.Montanari 's example in https://community.st.com/t5/stm32-mcus/how-to-implement-usbx-in-standalone-mode/ta-p/614435, and also referred to a CubeMX example for Device MSC which does use an RTOS (STM32Cube_FW_U5_V1.6.0\Projects\STM32U575I-EV\Applications\USBX\Ux_Device_MSC). I'm running this on an STM32U5 dev kit.There are no errors, Windows recognizes the USB MSC device, and a drive shows up. But something isn't working quite right, since Windows tells me to insert a disk, won't format the volume, and doesn't seem to recognize its size.I'm not quite sure yet where things are going wrong, but I thought I'd see if this configuration is expected to work or if I'm overlooking any other examples before digging further...
Hi,A bare-metal solution using the ST87M01-1301 modem (FW: v2.9.0) and a TCP connection to a remote server, with mbedTLS handling the TLS. We are experiencing an issue with one specific server (which is not under our management, making it very difficult to obtain server-side logs). The server does not respond to our TLS Client Hello at all. It does not send a TLS alert or close the connection; it simply leaves the socket open until our application timeout terminates the connection after 2 minutes.Here is what we have verified and tested so far:* The exact same Client Hello payload was copied and tested from a PC, and the server responds correctly with a Server Hello.* The exact same bare-metal implementation works with three other remote servers.* +CGCONTRDP reports an MTU of 1500. We have attempted to lower the "max_ip_frame_size" on the ST87M01 from 1600 down to 512 bytes, but it had no effect.* During PC test, if we transmit an invalid Client Hello, the server immediately terminates
Dear Sir/Madam,We have got below products " STM32F030C8T6 " from the authorized distributor and we found the label shows as below : Country of Origin: United Statis it the spelling error or other reason ? Is it the correct label ? when did it change the label format ? Will you have the relate documents with the PCN or the link ? Pls help to check and advise .Will be much appreciate it .Thank youSuki
I’m trying to implement USB mass storage class device standalone(no RTOS) on nucleo board STM32U575ZI-Q, using RAM for memory.I tried adapting these steps : but right now, in MX_USBX_Init(), inside ux_device_stack_initialize , at this point:#if UX_DEVICE_ENDPOINT_BUFFER_OWNER == 0 /* Obtain some memory. */ endpoints_pool -> ux_slave_endpoint_transfer_request.ux_slave_transfer_request_data_pointer = _ux_utility_memory_allocate(UX_NO_ALIGN, UX_CACHE_SAFE_MEMORY, UX_SLAVE_REQUEST_DATA_MAX_LENGTH); /* Ensure we could allocate memory. */ if (endpoints_pool -> ux_slave_endpoint_transfer_request.ux_slave_transfer_request_data_pointer == UX_NULL) { status = UX_MEMORY_INSUFFICIENT; break; }#endifit goes : status = UX_MEMORY_INSUFFICIENT;Because of that, ux_device_stack_initialize returns UX_ERROR; witch i think causes Hard fa
Dear ST Support Team,I am following the procedure described in AN5464 – Position control of a three-phase permanent magnet motor using X-CUBE-MCSDK. As mentioned in Section 5.8, MC_StartMotor1() performs the encoder alignment and zero-reset procedure, and MC_GetAlignmentStatusMotor1() is used to check whether the alignment has been completed.I have verified that the encoder Z (index) signal is working correctly and have checked the Z-index pulse separately. However, the alignment function call is still failing, and the alignment is not completing as expected.Could you please help me identify what could be causing the alignment function to fail even though the Z-index signal is working correctly? Please also suggest which parameters, configuration settings, or firmware sections I should check for debugging this issue.Reference: AN5464, Section 5.8 – API Usage.Regards,Prathmesh
Hello ST Support,I am using an STM32H743VIT6 on a custom PCB. The PCB has already been fabricated, and I discovered that the VBAT pin is left unconnected (floating).My application does not use RTC, LSE, backup registers, backup SRAM, or battery backup functionality.The MCU is continuously powered from 3.3 V through VDD.I would like to confirm whether leaving VBAT unconnected can affect normal MCU operation while VDD is present, specifically:CPU execution Flash operation GPIO DMA SAI/I²S UART USB interrupts timers normal peripheral operationI understand from RM0433 that the VBAT domain contains the RTC, backup registers and backup SRAM, and that when VDD is present the backup domain is supplied from VDD.The reference manual also states that VBAT may be connected directly to VDD, and that VBAT functionality is used when VDD is not present.My specific question is:With VDD continuously present and no requirement for RTC/backup functionality, is an STM32H743VIT6 with VBAT left floating guar
Using STM32CubeIDE v1.17 (STM32CubeMX v6.13) to edit IOC file and generate code...Previously when working with STM32H563 I selected X-CUBE-FREERTOS under Middleware, added tasks, generated code, and saw expected code in app_freertos.c for tasks.Now starting to work with STM32G491. Under Middleware I see FREERTOS but no X-CUBE-FREERTOS. After adding a task and generating code, I see nothing in app_freertos.c for the task. What is the difference between FREERTOS and X-CUBE-FREERTOS?Why don’t I see X-CUBE-FREERTOS when working with STM32G491?
Hi All,So I have an STM32F469 on a PCB I’ve designed with a CS4270 audio codec. I am currently working on an I2C driver to initialize the codec (I am using code from Phil’s lab’s video on writing an I2C driver for the CS4270 - video here), however I seem to be running into a “Bus, memory management or usage fault (FORCED)” and an “Instruction access violation (IACCVIOL)” during an I2C register read function.Here is the codec init file. The faults happen in this function call:i2cStatus = CS4270_RegRead(CS4270_REG_DEVICEID, &deviceID);During one of the debug sessions I decided to “step into” every single instruction from the CS4270_RegWrite function (also going through all the HAL functions underneath) and surprisingly the function returned a HAL_OK, which puzzled me and lead me to believe there maybe some kinda timing issue somewhere, which doesn’t manifest itself when breaking down the instructions one by one. Something worth noting is that initially I had initialized the I2C1 modu
Hi all, for minimum wake time I want to use UDP with DTLS.However, I wonder if it is OK to keep the Socket open for a longer time (not closing it ever)? Even during PSM?Opening the DTLS-Sockets costs 2 seconds (handshake) and energy, for a Raw-Socket it is almost zeroDTLS: Init->Wait->Use[000000]> AT#SOCKETCREATE=5,0,UDP,0,60,60,9,0,0[000116]< #SOCKETCREATE: 0[000118]< OK[000000]> AT#DTLSCONNECT=5,0,xxx.xxx.xxx.xxx,pppp[002011]< #TLS: 3,0x00A8,2048,0[002012]< OK[000000]> AT#IPSENDUDP=5,0,xxx.xxx.xxx.xxx,pppp…Raw[000011]< #SOCKETCREATE: 0[000012]< OK[000000]> AT#IPSENDUDP=5,0,xxx.xxx.xxx.xxx,pppp…Thanks for any helpful infos,Jo
Hello ST Community,I am planning to use the NUCLEO-G474RE (STM32G474RE) for controlling a 3-phase AC motor using STM32 Motor Control Workbench (MCSDK).I would like to know: Is the NUCLEO-G474RE supported for 3-phase AC induction motor control using Motor Control Workbench? Can Motor Control Workbench generate the required 6 PWM signals for a 3-phase inverter? Does MCSDK support 3-phase induction motor (ACIM) control on STM32G474RE? If yes, which control method is recommended—V/f, sensorless FOC, or encoder-based FOC? Does ST provide a ready-made firmware/example project for this setup? What ST power stage/inverter board would you recommend for testing with the NUCLEO-G474RE? My expected application is a 3-phase AC motor drive, and I am evaluating the STM32G474RE for production use.Thank you.
3x VL53L0X shows no readings For an application I need 3 VL53L0X TOF sensors. The code can be used to successfully boot the three sensors. However, only the third sensor provides a measured value. If the sensors are used individually, boot and measurement is OK.Do sensor 1 and sensor 2 have to be activated by function
I am currently using the STM32U599VI in our application and are attempting to achieve the low-power performance specified in the datasheet.According to the device specifications, the low power standby mode current consumption is expected to be approximately 195 nA under the specified test conditions. However, in our application, we are observing a significantly higher current consumption in standby mode, approximately 5-6 mA.I would appreciate support in identifying the possible causes of this high standby current and guidance on the necessary hardware and software configurations required to achieve the expected standby current consumption.
Dear supplier For P/N: STP5NK100Z certification we see just cocPlease mark the reason why you only provide a certificate of conformity (COfC) 1.2.3.4 which is correct ? 1. standard parts manufactured to a standard part specifition.2. Part number is part of a standard part manual3. TSO authorization4. None of the above reasonsTHANKSCHERRY
I found an overview of ST’s ToF sensors at https://www.st.com/en/imaging-and-photonics-solutions/time-of-flight-sensors.htmlBut I miss the VL53L5CX in the picture.(Just in case someone wants to keep it up to date…I need no solution or any answer, but I can not select anything else than a question when creating a topic.) BR Klaus
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.