User Activity

Hello All,,  I am using STSAFE-A110 with stm32f429zit6 for secure boot, I want sample code / library for the same. Also my another query is will I have to sign the firmware using openssl externally. can anyone provide me complete step to finish the s...
Hello all, I am using STM32H747 in my project, previously I was using HAL library for my project, but now I want to shift my code to standard peripheral library, my question is do STMH7 series support to standard peripheral library if Yes then can an...
Hello,I am using STM32H747 Discovery board in that I am using TFT display using LVGL in code my RAM is taking space upto 250 KB and my code is going in hardfault_handler(); Can anyone suggest me the solution
Hello all,Currently I am working on STM32H747 discovery board in that working on touch of MB1166 board,The touch controller is FT6336U so I want slave address of the touch controller and sample code for the same thanks 
Hello Guys, Currently I am using Parallel RGB888 TFT display with resolution 800X480 in which I am using STM32F429ZIT6 controller using LTDC with DMA2 and I am printing whole RED color on display but display showing lines. My question is as I am not ...
Kudos given to