cancel
Showing results for 
Search instead for 
Did you mean: 

Standard Peripheral Library for STM32H7

tobbymathew
Associate II

Hello all,

 

I am using STM32H747 in my project, previously I was using HAL library for my project, but now I want to shift my code to standard peripheral library, my question is do STMH7 series support to standard peripheral library if Yes then can anyone share me the SDK for the same

 

 

Thanks!!!!

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello @tobbymathew ,

There is no SPL library for H7. If you mean by that using low level driver you can use LL implementation available in HAL:

SofLit_0-1734526072523.png 

But not all peripherals have this implementation: FDCAN as an example.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2

The Standard Peripheral Library (SPL) was the predecessor of HAL.

I think SPL was discontinued (replaced by HAL) long before the H7 series was introduced.

 


@tobbymathew wrote:

I was using HAL library for my project, but now I want to shift my code to standard peripheral library


Why?

 


@tobbymathew wrote:

do STMH7 series support to standard peripheral library 


You're asking that question the wrong way around.

The real question: "Is SPL available for STM32H7?" - to which the answer is, NO:

https://community.st.com/t5/stm32-mcus-embedded-software/does-the-spl-is-available-for-stm32g-series/m-p/265995/highlight/true#M18065

https://www.st.com/en/embedded-software/stm32-standard-peripheral-libraries.html

 

mƎALLEm
ST Employee

Hello @tobbymathew ,

There is no SPL library for H7. If you mean by that using low level driver you can use LL implementation available in HAL:

SofLit_0-1734526072523.png 

But not all peripherals have this implementation: FDCAN as an example.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.