User Activity

Hi All,currently, we are using the VL53L1 ToF-Sensor im some of our products, which will be replaced with the VL53L5- and L7 sensor. Unfortunately, there is no support of user-defined ROIs in the ULD.Since in our application, a full, square-shaped fr...
Hi,i am using both the VL53L5 and L7 in a quite limited space, where the sensor need to run in the 8x8 continuous mode. Therefore, the thermal design is quite challenging.  So, my question is: what temperature does the sensor specifically deliver wit...
Hello,the VL53L5CX and L7CX ULD guides mention that a target status of 6 and 9 should be considered with a confidence of 50 %, while a comment in the api.h file says that  "5 & 9 means ranging OK", which gives the impression of a higher confidence ra...
Kudos from
Kudos given to