2024-08-24 7:42 AM
Hi,
Can somebody please suggest me a ToF sensor with signal sampling rate of atleast 1MhZ.
Thank you
Solved! Go to Solution.
2024-08-28 11:54 PM
The ToF sensors from STMicroelectronics measure the propagation time of the photons from the integrated laser to the integrated receiver using a proprietary method. An ADC would be far too slow for the short propagation times, which is why there is no sampling rate.
The ToF sensors also cannot work with external lasers.
Regards
/Peter
2024-08-27 11:38 AM
Sorry -
I don't know of an ST part that can help you.
-john
2024-08-28 12:13 AM
Regards
/Peter
2024-08-28 10:55 AM
HI Peter,
Thanks for the reply.
2024-08-28 11:54 PM
The ToF sensors from STMicroelectronics measure the propagation time of the photons from the integrated laser to the integrated receiver using a proprietary method. An ADC would be far too slow for the short propagation times, which is why there is no sampling rate.
The ToF sensors also cannot work with external lasers.
Regards
/Peter