Skip to main content
Wadeva
Associate III
September 23, 2024
Solved

My STM32 device is overheating and has malfunctioned

Hello,

We’ve designed a device that uses an STM32 microcontroller to manage various features such as I2C, UART, ADC, IWDG, DMA, Flash memory handling etc. After running smoothly for a month, the device began malfunctioning, drawing 220 mA of current and heating up noticeably. I’m trying to determine the root cause of this issue. Could you provide insights into the possible reasons for this behavior?

Thank you.

This topic has been closed for replies.
Wadeva
WadevaBest answer
Associate III
September 25, 2024

Hello everyone, after reviewing our design, I discovered an unprotected pin that is connected to the chassis ground of the device. I’ll need to check if there are any other similar pins. It must be the problem.

 

20 replies

Andrew Neil
Super User
September 23, 2024

@Wadeva wrote:

Could you provide insights into the possible reasons for this behavior?


  1. A hardware failure in your external hardware
  2. A design error (software and/or hardware) over-stressing the part (or allowing it to get over-stressed).

 

For anything more specific, you're going to have to give a lot more detail!

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Wadeva
WadevaAuthor
Associate III
September 23, 2024

Dear Andrew,

Our design involves numerous components, making it difficult to specify each one. We are using the STM32G070CBT microcontroller.

I’m unsure what might be causing this issue, as all peripherals and features seem to be functioning normally—no signs of overcurrent or short circuits. However, I’m curious if this type of malfunction could be related to something specific, like overcurrent in a peripheral or excessive heat.

I will try to narrow down the issue by individually testing each peripheral and reviewing our software.

 

Andrew Neil
Super User
September 23, 2024

@Wadeva wrote:

Our design involves numerous components, making it difficult to specify each one.


Your design should fully specify all of them!

 


@Wadeva wrote:

I’m curious if this type of malfunction could be related to something specific, like overcurrent in a peripheral or excessive heat.


Yes - as I said, over-stressing the part.

The primary result of overcurrent is overheating!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
TDK
September 23, 2024

Look for possible places where the chip might have been overstressed, perhaps on powerup, perhaps by an external component through a long (inductive) wire, or ESD damage, or something of the sort.

When the chip is overstressed, the protection diodes can fail and cause the chip to sink a massive amount of current, sometimes while otherwise working okay.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Wadeva
WadevaAuthor
Associate III
September 23, 2024

Thank you TDK.

I will look and search with my team and tell you if we found the main reason.

 

Associate III
September 23, 2024

How do you have your output pins configured?

Just try to config all as open drain with pull-up, be carefully that e.g. pwm stages may stop working correctly. If all pins are going high, you can exclude that your periphery is broken.

Next tests and other cases are more difficult, but also more rare I guess.

Wadeva
WadevaAuthor
Associate III
September 23, 2024

 

We are using both push-pull and open-drain configurations on different pins. Additionally, some pins have internal pull-up or pull-down resistors activated.

 

An interesting test. I will give it a try but as you said my problem might be the rare one.

AScha.3
Super User
September 23, 2024

Hi,

in such "cases" , i just power the board and watch it with an IR cam ->

you see, where the power goes -- or only cpu gets hot, then you damaged it (if your program was working before, without heating, otherwise try the simple test setup with all pins unused or inputs.)

If you feel a post has answered your question, please click on " Best Answer ".
Wadeva
WadevaAuthorBest answer
Associate III
September 25, 2024

Hello everyone, after reviewing our design, I discovered an unprotected pin that is connected to the chassis ground of the device. I’ll need to check if there are any other similar pins. It must be the problem.

 

Associate III
September 25, 2024

@Wadeva wrote:

Hello everyone, after reviewing our design, I discovered an unprotected pin that is connected to the chassis ground of the device. I’ll need to check if there are any other similar pins. It must be the problem.

 


In this case, you better provide more information. In special the (important parts of the) schematic. A new thread is a good idea - with linking here to it.

Andrew Neil
Super User
September 27, 2024
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.