Hello, how to know ram memory usage using debugger, to check where memory is used. This is without FreeRTOS or CMSISI know freeRTOS has TaskGetStackHighWaterMark()
Hi,1. is there any tool (GUI) to update program using executable?2. How to have different modes of programming? (UART/ USB/ sd card)3. Bootloader mentions: USB OTG FS (PA11/12) in Device mode (DFU: device firmware upgrade). Can external HS phy in FS ...
hello,
sd card write on f469 discovery is working. and now referring to msc_standalone example (which works alone), usbd_storage_if.c file is matched and usb mass storage selected from MX tool.
But i cant see the drive coming. can i know steps have ...
Hi, Im referring F429 eval board fmc sram code. For Nucleo f439, I changed to bank 1 and bank addr=0x60000000 with R/W from e.g. and init from MX tool.The issue I see is on receive, the values are not the same (compared to TX) when buffer size>128
Hi, I was trying to have microSD logging with F439 Nucleo. I can't see example with mentioned board. Please let me know:1. example for mentioned board to log data in microSD2. I tried configuring SD-4 bit, but couldn't identify the pins intialized in...
questions: 1. is the .elf ok, I haven't changed anything to have different file2. is boot1 pin changes needed?3. Is any change if CubeProgrammer needed for PID, VID for USB DFU?
Hello, I got USB FS for MSC on board working for F439 Nucleo. Now try is for USB3300 HS with Waveshare board.I configured through MX and updated usbd_storage_if similar to FS changes. But I dont see USB getting detected in Windows.Is this driver issu...
CubeProg logs for USB DFU, verify program is failing 18:47:37 : UR connection mode is defined with the HWrst reset mode
18:47:37 : USB speed : Full Speed (12MBit/s)
18:47:37 : Manuf. ID : STMicroelectronics
18:47:37 : Product ID : STM32 ...