User Activity

Hi, I got a problem with the reception using USART7. I'm using it in the interrupt mode but the problem is that the data in the buffer is not coming well. I'm connecting STM32F407 board with the STM32F746 using UART. When the F7 transmits, there's no...
Hi, I'm using the USART3 on interrupt mode with the STM32F407 chip and I cant figure out why the recive function is not working.I'm transmiting from a STM32F7 a buffer like this: "$en:X# to the F4 but this buffer never arrives when debugging. I'm sur...
Hi, I want to conect an external MCU to the STM32F746 DISCO using UART but I dont know how to use another UART other than the one used for communication with the PC.
Hi, I'd like to use a code from javascript in the STM32F746 DISCO. It's a radar that receives data from an ultrasonic sensor. The code for the radar was made using processing and I want to show it in the STM screen but I got no idea.Here is the code ...
Hi, got a problem opening the .ioc.It shows me this error.  
Kudos from