User Activity

The conclusion is that setting filters and interrupts on FIFO0 leads to exception handlingFDCAN1_IT1_IRQHandler.The reason for this behavior is an error in the file. startup_stm32g431cbtx.s ERROR ...word ADC1_2_IRQHandler.word USB_HP_IRQHandler.word ...
Looking through the RM0440 and the datasheet on the STM32G4,I can't find information on the maximum recommended frequency for modulCANFD.Or it may be the same as for microcontroller up to 170 MHz?HSE 8mhz -> PllM /2 -> PLLx85 /R /2 ... APB1 /1 -> PCL...