User Activity

Whenever I set the SMPS Clock Mux to HSE /4 /2 = 4 I can save the project without errors but whenever I reopen the ioc file I get a warning that there is a clock issue that needs to be fixed.  I go into the clock configuration and it's bee reset to H...
I've been having a lot of trouble getting all of the online BLE examples to work and was hoping someone could steer me in the right direction.  In every example they state that the RFWKP Clock Mux should be set to LSE but whenever I do that the main ...
Hello, reaching out to see if anyone can provide some thoughts on a project I'm working on.  The project works but though I'm a longtime Arduino developer this is my first STM32 project - so not 100% sure of some of the parameters I've chosen are the...
I have a custom board with an STM32WB55CEU6 that I'm programming using the STM32CubeIDE.  I'm struggling with getting the ADC to work in DMA mode.  I can connect via SWD and the while loop runs fine but HAL_ADC_ConvCpltCallback is only triggered once...
Hello, I'm configuring an STM32WB55CEU6 in STM32CubeIDE and am setting up the BLE part now and I noticed that the IDE only let's me setup 5 characteristics per service.  In my application (a remote control) I need about 15 characteristics.  Is there ...
Kudos given to