I'd also love an answer for this. This could be a very useful features but there doesn't seem to be any documentaiton about it; only a few users here on the forums attempting to use it (using .bat files?) and invariably running into problems along th...
@TDK Copy that - so has internal ticket reference # 170481 received any updates that can be shared, or has the ticket been closed/resolved?Regarding the issue I mentioned, yes, I have had ADC3, ADC4, and ADC5 active in my project. So I will open anot...
Hello @Semer CHERNI and company; any updates with this? The issue was first reported in January, it is now last day of July. I have the latest version of CubeIDE (1.16.0) and the built-in MX will not allow me to change ADC345 Clock Mux. This looks li...