User Activity

This Topic is used for Wireless Charging solution 1.Mcu C drive code: GitHub - STMicroelectronics/STWirelessCharging-C-Drivers: Standard C platform-independent drivers for wireless charging ICs 2. Python drive code, check attach file "Python_FT260_S...
Many customer face dongle driver issues, most because Unable to load DLL 'HidDongle.dll'.  @sjones i post your request in the forum. Key points: This eval board has an on board FT260, which should take care of the I2C to USB (HID) interface without a...
STWBC86 TX can be use for bi-directional communication, when rx send PP-packet as QI defined, STWBC86 update to 1251 version and use GUI to read i2c reg address 0x0100, and it can read RX PP-packet. https://github.com/STwirelesscharger/STSW-WPSTUDIO/...